Part Number: DRV8842-EP Other Parts Discussed in Thread: DRV8842 Hi All,
I am using a DRV8842-EP in my design. I have done design as per the recommended schematic. I am using this DRV8842-EP for driving a solenoid vlave which consumes 0.650 A of current…
Part Number: DRV8842-EP Hi Team,
I am using DRV8842-EP to drive a solenoid valve. I am making the circuit as per the reference diagram provided in the data sheet. I have doubt regarding a capacitor value. In the datasheet of DRV8842-EP ,t he typical…
Part Number: DRV8842-EP I would like to get some more clarity on the working of the DRV8842-EP. I have few doubts regrading H-Bridge operation configuration.
In the above image - direction of current flow shown by 1 is for the condition when IN1 …
Part Number: DRV8842-EP Dear Design support team.
It is designed as below. VM voltage is 30V. this means DC motor operating voltage is 30V.
Generally condition, I will control the motor using only primary driver IC.
The redundant driver IC…
Part Number: DRV8842-EP Other Parts Discussed in Thread: DRV8251 Hello, i need the parameters such as dead time, slew rate, rising and falling times for calculating power dissipation of h-bridge structure. I want to calculate switching loss and dead time…
Part Number: DRV8842EVM Other Parts Discussed in Thread: DRV8842-EP , DRV8842 , Hello,
This is a question regarding current regulation of DRV8842-EP.
We are now testing the current regulation function of DRV8842 on the evaluation board.
The…
Part Number: DRV8842EVM Other Parts Discussed in Thread: DRV8842-EP , DRV8842 , , DRV8872-Q1 , DRV8876 Hello,
This is a question regarding current regulation of DRV8842-EP.
We are now testing the current regulation function of DRV8842 on the evaluation…
Hi Renan,
There is the DRV8843-EP which is an enhanced package version of the DRV8842. It can support defense, aerospace, and medical applications. It also supports military temperature range (-55C to 125C). Unfortunately, this device is out of stock…