Part Number: DRV8842EVM Tool/software: Hi Team,
Customer test DRV8842EVM and the VM input is 32V and the I0~I4 is all "1" to set full scale current output.
However, if no loading, the output waveform is no problem.
While loading attached, the…
Part Number: DRV8842EVM Hi, Im having issues with the DRV8842EVM driver software not being able to detect a labview runtime engine on my stsem, however I have the 2014 engine installed.
I have tried moving the runtime into the same folder as the driver…
Part Number: DRV8842EVM Hello,
I need to drive much larger current than the ISEN resistor R5=0.2 allows.
I know the limits of the IC.
What are the limits of the EVM?
Can it handle the full 5A continuous?
Thanks,
Emmett
Part Number: DRV8842EVM Other Parts Discussed in Thread: DRV8842-EP , DRV8842 , , DRV8872-Q1 , DRV8876 Hello,
This is a question regarding current regulation of DRV8842-EP.
We are now testing the current regulation function of DRV8842 on the evaluation…
Part Number: DRV8842EVM Other Parts Discussed in Thread: DRV8842-EP , DRV8842 , Hello,
This is a question regarding current regulation of DRV8842-EP.
We are now testing the current regulation function of DRV8842 on the evaluation board.
The…
Part Number: DRV8842EVM Hi.
Customer has tested DR8842EVM and found out, that OCP condition can be removed by nRESET signal and also by nSLEEP signal.
Based on datasheet OCP recovery can be done only by power cycle and nRESET signal.
Can you please…
Part Number: DRV8842EVM Does anyone has the schematic diagram of CPG005_DRV88xx Evaluation Modules? because I am goin to use a group of DIO from my own MCU module to connect to the IN1,IN2, I0~I4, DECAY, nSLEEP and nRESET pins on this CPG005_DRV88xx Evaluation…
Hi Claus,
In the GUI there is a pulldown that allow changing com ports. Please make sure the correct com port is selected prior to connecting.
Can you provide a screen capture of the GUI and a screen capture of the device manager showing the Ports…