Part Number: DRV8845 Tool/software: Hello Experts,
I am currently working on a project to drive three DC motors using the DRV8845 motor driver.
I am experiencing an issue where Motors 1 and 2 are functioning correctly, but Motor 3 is not working at…
Part Number: DRV8845 Other Parts Discussed in Thread: DRV8849 , Hello,
I do not see the package details within the datasheet, nor on the TI pacakge webside for the RHH (VQFN 36) package.
Woudl you kindly provide a drawign which shows the detailed…
Part Number: DRV8845 Other Parts Discussed in Thread: DRV8849
Tool/software:
The DRV8845 is fully pin-to-pin compatible and software compatible with the Allegro A3988, A5988, A5989, and Relmon MS3988 and MS3989. This means that you can directly replace…
Part Number: DRV8845EVM Other Parts Discussed in Thread: DRV8845 We are using stepper motor drive IC DRV8845 for driving 2 phase stepper motors.
There is a huge humming sound during the rotation of stepper motor.
Please guide me to resolve the humming…
Part Number: DRV8845 Tool/software: Hello Team,
My customer is evaluating DRV8845, and we are unsure if the unused driver related pins can be left floating or if there is a certain termination that needs to occur. Specifically, they will not be using…
Part Number: DRV8845 Tool/software: Can we operate each Full bridge individually and simultaneously? because I need to control four DC motors simultaneously with different PWM duty ratios
Part Number: DRV8845 Hi,
We have used DRV8845RHHR in our project to drive stepper motor having following specifications.
1) No of phase - 2
2) Phase voltage - 6.6V
3) Phase current - 1A
4 ) Phase resistance - 6.6ohms
5) Size : NEMA 17
…
Part Number: DRV8845 Tool/software: DRV8845 is linear motor driver. If VM is more larger than motor voltage, motor driver will be hot.
Could I add SENSE1 and SENSE2 voltage feedback to CC buck power for supply DRV8845 VM?
Part Number: DRV8845 Other Parts Discussed in Thread: DRV8912-Q1 , DRV8849 Hi Team,
Please help to suggest a solution for BU24033GW replacement.
Thanks.