Part Number: DRV8845EVM Other Parts Discussed in Thread: DRV8845 We are using stepper motor drive IC DRV8845 for driving 2 phase stepper motors.
There is a huge humming sound during the rotation of stepper motor.
Please guide me to resolve the humming…
Part Number: DRV8845 Other Parts Discussed in Thread: DRV8849
Tool/software:
The DRV8845 is fully pin-to-pin compatible and software compatible with the Allegro A3988, A5988, A5989, and Relmon MS3988 and MS3989. This means that you can directly replace…
Hey Kiran,
I recommend you test it and find in your system with this motor and a given load how much current you need, and how much the motor heats up with that given current. I think you'll find the motor capable of >6.6V at 0.7A without issue. Motors…
Part Number: DRV8962EVM Other Parts Discussed in Thread: DRV8962 , DRV8845EVM , DRV8462 , DRV8962VEVM , DRV8262 Hi,
We are trying to use DRV8962EVM and its 4 current sense signals as feedback signals in closing the current loop in a stepper motor control…
Hi Allen,
I am a bit confused by your question.
Allen Huang said: If VM is more larger than motor voltage, motor driver will be hot.
VM is the "motor voltage". As long as the motor voltage supply is within recommended operating conditions there…