Part Number: DRV8847
Hi,
This question is regarding the protection circuitry inside the DRV8847PWPR.
I have been using the DRV8847PWPR for some time to activate latching solenoids via SSRs, allowing a common H-bridge IC to control multiple SSRs…
Part Number: DRV8847 Tool/software: Existing KA3100 to replace DRV8847.
We have use DRV8847 in our instrument for thermal printer driver motor,
DRV8847 use 2-Pin Interface interface
refer attached print image of existing(KA3100) and New (DRV8847…
Part Number: DRV8847 Hi
I hope this explanation is not confusing — I will try to keep it as simple as possible. I am hoping this issue can be solved with a simple logic or mode-shift solution.
I am using the DRV8847PWPR in I²C mode to control up to…
Part Number: DRV8847
Tool/software:
Hi Team,
Please recommend a stepper motor driver IC. Please refer to the attached motor specification sheet.
Thanks
Part Number: DRV8847 To the person in charge
Please send me "Total Power Dissipation vs Free-Air Temperature" of DRV8847PWR .
It is not listed in the data sheet.
Best Regards
Shingu
Part Number: DRV8847 Tool/software: Hi
I am using the DRV8847PWPR to control some 12V latching solenoids. The 12V power provided to the DRV8847PWPR is being supplied from Li-ion Battery. Do to the coil in the solenoid, do we need to add any additional…
Part Number: DRV8847 Other Parts Discussed in Thread: DRV8835 , Tool/software: Hi, I am looking for the replacement with minimal board changes for the IC BA6845FS to drive Motor MLT-288 bipolar stepper motor. help me to find the same. In TI Cross reference…
Part Number: DRV8847 Tool/software: Hi team,
My customer is using DRV8847, and they want to use nSLEEP to reset. They are asking how long should the nSLEEP low signal last for IC to detect and enter sleep mode.
I saw a tSLEEP in the datasheet, and…
Part Number: DRV8847 I am using DRV8847 with MODE=1 and IN3=1. At PWM frequencies below 2kHz, the device operates as expected. Above this frequency the outputs that should be L have a signal that is in opposite phase to the H outputs (ref Table 5 in datasheet…