Part Number: DRV8850
Hi team,
Our customer wants to know whether the LDOOUT pin and LDOFB pin can connected to nothing when the LDOEN pulled low.
Thanks and best regards
Ella
Part Number: DRV8850
P.3, Chapter 5 - Pin Configuration and function
Table error (Package top view is correct):
(1) VCC Pins should be 18,19,20.
(2) OUT2 Pins should be 21,22,23.
Part Number: DRV8850 Hi
1.
LDO function of DRV8850 is not used in the application.
Could you please tell us adequate termination of LDOEN, LDOFB and LDOOUT?
To saving power, could they be left open?
2.
We will need only forward driving.
Is the following…
Part Number: DRV8850
Hi,
we are using the DRV8850 to drive a linear motor. When designing the PCB, the following question arose:
The chip has this VPROPI pin that is connected via 1k to GND in our application according to TI proposals. As we don’t need…
Part Number: DRV8850 Hi
For brushed DC motor opeartion, use of VM=2V is required.
Motor specification is following.
VM=2V
Istart=2A
Ilock=4A
In addition, motor lock detection function should be implemented in system.
DRV8850 has VPROPI, so current…
Part Number: DRV8850 Hi,
My customer is conducting failure analysis on a unit of their product that is about to go into production. They see a small amount of current leakage on VPROPI of the motor driver (DRV8850) when enabling the motor but without…
Part Number: DRV8850
I've looked around the TI website for the package drawing for the DRV8850, since it's not in the datasheet, and I found the drawing. However, the drawing refers to a separate sheet for the thermal pad, but there is no separate…
Part Number: DRV8850 Hi
DRV8850 has no brake function but it could be possible to INxL to high and INxH to low.
Is it correct?
If yes, is it possible to operate brake with EVM?
BestRegards
Part Number: DRV8850 Other Parts Discussed in Thread: TPS28225 , DRV8702-Q1 , DRV8704 , DRV8703-Q1 , DRV8701 , DRV8320 , DRV8301 , DRV8323 Hi
We are looking for H bridge gate driver for Nch FET (All N ch FET).
We need device that drive external FET.
So, DRV…
Part Number: DRV8850 We're not going to use the LDO in the DRV8850, so we'll leave the LDOEN pin open and let its internal pull-down disable the LDO. Given that the LDOFB pin is an input, what should we do with it in this case? Leave it open? …