Part Number: DRV8860 Hi Experts,
My customer is wondering about the range of CLK frequency of DRV8860. From the datasheet, is the max CLK frequency 1/tclk ?
Could you pls help on it? Thank you!
BR,
Skylar
Part Number: DRV8847 Other Parts Discussed in Thread: DRV8860 , , DRV8214 , DRV8234 Hi team,
I have a customer requesting something similar to the DRV8860 but with an I2C interface for driving solenoids. I saw that the DRV8847 is the only stepper motor…
Part Number: DRV8860 Hi Team,
customer is considering using DRV8860A for solenoid and LED control.
They have following question:
is the DRV8860A capable of sourcing the small current within the order of 5, 10 and 20 mA’s?
Is there a AP note for…
Part Number: DRV8860 Other Parts Discussed in Thread: DRV8962 Hi Tier
My customer want to use DRV8860PWP to drive four kind of Solenoid.
Could you help me evaluate whether DRV8860PWP is suitable for use here.
Solenoid list:
Part number…
Part Number: DRV8860 I have an application where the DRV8860 is being used to activate some solenoid valves. VM = 24V and is fed to the DRV8860 through a high-side switch (TPS1H100).
We are trying to understand what happens if the 24V voltage feeding…
Part Number: DRV8860 Hi Team,
Our customer is using DRV8860 and found 2pcs failure out of 5000pcs without normal output compared with good device, some waveforms captured are as below. Can you help to check what's the possible reason for these two failures…
Part Number: DRV8860 Hi.
in designing a driver for 8 solenoid valves that uses DRV8860 I am asking if I have to consider to add at every utput a freewheeling diode in parallel with a resistor to act as a freewheeling diode to dissipate the energy stored…
Part Number: DRV8860 Hello,
1. Please check whether the schematic design of the accessories is reasonable?
2. The two DRV8860 are not connected to the load. Why is the FAULT pin not pulled down?
3. How to test the open circuit protection function…
Part Number: DRV8860 Hi team,
My customer used DRV8860 to drive 3 LED. DRV8860 SPI interface directly connect MCU I/O. We can see below SCH.
But after board working 1 year, we saw 25% board broken. We can see the broken board in below pic and DRV8860…
Part Number: DRV8860 Hi,I found that after each reset of the fault register, the first reading of the fault register was wrong, and there was a problem of shifting to the left, and the reading from the second time onwards was correct.
1. Test conditions…