Part Number: DRV8870 Hello,
We have an electronic board developed a few years ago that uses the DRV8870DDAR component. The old boards have not shown any issues. However, during a new production run, the new boards are not working correctly. It seems…
Part Number: DRV8870 Hi,
We use DRV8870 for our BLDC driver, and now, we test the motor stall function
The drvier is fault after about 10s the motor stall;
We release the motor rotor and DRV8870 can't automatic Fault Recovery, but the datasheet…
Part Number: DRV8870 Other Parts Discussed in Thread: DRV8251A , DRV8231A Hi Expert,
Regarding the current‑limit feature of the DRV8870, the datasheet only specifies the op‑amp’s range as 9.4 V to 10.4 V, but it does not give the comparator’s accuracy…
Part Number: DRV8870 hi expert
When we were testing a circuit driven by DRV8870, we encountered an abnormal output situation in low-temperature environments. The circuit worked normally at normal temperatures. Around minus 20 degrees Celsius, the current…
Part Number: DRV8870 Other Parts Discussed in Thread: DRV8424E , DRV8828 , DRV8829 , DRV8436E Tool/software: Hello,
We using DRV8870 driver web tensioning application.
In this application we we driving motor in reverse direction and externally it…
Part Number: DRV8870 Dear TI Team,
We are using the DRV8870 device since many years on one of our product.
It's driving a small DC motor.
The DRV8870 is suppyed in 24V, and its commands are in ON/OFF 0_5v signals on its 2 inputs (IN1 and In2) to…
Part Number: DRV8870 Tool/software: do you have new PCN for label , left is new coming goods, right is old goods, but label is different. please help check it 。
Part Number: DRV8870 Other Parts Discussed in Thread: DRV8231A Tool/software: Hi Team
I have two question about DRV8870.
1. do H bridge need a reverse current protection? or it default need a reverse current so VM need to handle reverse current…
Part Number: DRV8870 Tool/software: Hello,
We have used this part for many years to drive a small DC/DC converter. The inputs are complementary square waves without deadtime created from a 555-timer. According to the datasheet, 220 ns of deadtime should…
Part Number: DRV8870 Other Parts Discussed in Thread: DRV8874 , DRV8231A Tool/software: Hi team,
May I get the SOA curve of MOSFET for DRV8874 and DRV8231A?
BR
Amber