Part Number: DRV8871-Q1 Hi, team.
The data sheet has the following description, is 800 ns typo?
"The voltages applied to the inputs should have at least 800 ns of pulse width to ensure detection. Typical devices require at least 400 ns. If the PWM frequency…
Part Number: DRV8871-Q1 I have some problem in controlling EV's inlet lock actuator control with DRV8871-Q1.
The lock actuator from Phoenix. The lock actuator can be controlled external DC power supply. It is not controlled with internal power source…
Part Number: DRV8871-Q1 Other Parts Discussed in Thread: DRV8872-Q1 , , DRV8871 Hi~
Customer is looking for high temperature operating motor drive which can support up to 120deg.
I found proper device DRV8871-Q1(DRV8872-Q1) on web site, but I don't have…
Part Number: DRV8871-Q1 Other Parts Discussed in Thread: DRV8871 Hi Team,
Is there an EVM available for the DRV8871-Q1? Need one urgently if so.
If not, what do you recommend to use to showcase the device?
Thanks,
Jared
Part Number: DRV8871-Q1 Hi Team,
I am trying to understand the power dissipation of the DRV8871-Q1 in more detail. There is a statement in the datasheet that specifies switching the inputs at 200kHz compared to 20kHz causes 20% more power loss.
Is there…
Ryan,
There is nothing like the DRV8908-Q1 that can support this frequency. You would have to consider standalone drivers with external PWM like the DRV8871/72-Q1 or DRV8876-Q1.
Regards,
Ryan
In the mean, I made also measurements with 350uH,and I tested different samples.
The 350uH measurements (dI/dT = 40mA/us at 12V) confirm the "constant delay" assumption: With Vref=3.3V, the bridge trips 4.6us after IPROPI rises above 3.3V.
…
Part Number: DRV8871 Hello guys,
One of my customers is considering using DRV8871 for their new products.
They have the following questions about DRV8871. Could you please give me your reply?
Q1. Iout (VILIM) variation of DRV8871 at 1A output is shown…
Hi Alvin,
We will have to investigate this the frequency of the internal charge pump. Expect an answer by Thursday.
Yes, the DRV8870, DRV8871, DRV8872, and DRV8872-Q1 have spread spectrum integrated.
What type of support document are you looking for? …