Part Number: DRV8872-Q1 Other Parts Discussed in Thread: DRV8872 Hi there,
has the DRV8872-Q2 any protection against feedback currents (e.g. loss of supply voltage)?
Or is it recommended to use external components for protection on the output paths…
Part Number: DRV8872-Q1 Other Parts Discussed in Thread: DRV8876-Q1 , DRV8874-Q1 Hi there,
Does the device also report (driving nFault low) when I_TRIP has been reached or really only when I_OUT is greater than I_OCP?
Thanks in advance for your help…
Part Number: DRV8872-Q1 Other Parts Discussed in Thread: DRV8872EVM Dear expert: Question1: What's the max voltage of pin out2, 12.7V or 50.7V? Considering VM is 12V in my application. Continuous phase node pin voltage (out1,out2) is found to be VM+0…
Part Number: DRV8872-Q1 Hello team,
Could you tell me a designed value of thermal shutdown about DRV8872-Q1? I would like to know the maximum value of TSD.
Best regards, Ochi
Part Number: DRV8872-Q1 Hi team,
How to set the protection trip level, when using DRV8872-Q1 in On-Board Charger application to lock the charging gun?
I notice that on datasheet, the overcurrent protection trip level varies from 3.7A to 6.6A, range…
Hi Michael,
The DRV8872-Q1 does have short to supply or ground protection on the outputs. If an output is short to VM and enabled low, or an output is short to GND and enabled high, an overcurrent event will occur.
The nFAULT pin should signal a…
Part Number: DRV8872-Q1 Other Parts Discussed in Thread: DRV8872 , DRV8412
I have some questions.
1. As shown below, using DRV8872-Q1 to connect BLDC with built-in speed controller. Is it right?
2. If it is not available, do you recommend…