Part Number: DRV8872-Q1 Hello,
I understand DRV8872-Q1 uses Cu wires, but has DRV8872-Q1 already been qualified for AEC-Q006? If not yet, would you please tell me when it will be?
Best Regards,
Yoshikazu Kawasaki
Part Number: DRV8872-Q1 Hi Champs,
My customer would like to calculate motor current when tOFF elapsed after Itrip reached as shown in attached.
Could you provide how to calculate the current under back_emif existing condition?
If there are some related…
Part Number: DRV8872-Q1
Hi Sir.:
I am verifying trip function. (Itrip =Vtrip/Risen)
But I can't get correct result.
(for example:)
VM =>24V
IN2 input signal => Logic High level
IN2 input signal => Logic Low level
winding…
Part Number: DRV8718-Q1 Other Parts Discussed in Thread: DRV8872 , , DRV8714S-Q1EVM Hi Team,
Do you have sample code for DRV8718-Q1? My customer want a code that with complex funtion of DRV8718 for their reference. My customer also has need like DRV8872…
Part Number: DRV8872-Q1 Hi Team,
My customer would like to calculate power dissipation with below use case.
- Vin : 6.5V
- Motor Current : 250mA
- Duty : 10%
- Motor resistance : 9ohm(min), 14ohm(typ), 22ohm(max)
- Ta = -40deg to 125deg
To calculate Power…
Part Number: DRV8872-Q1 Dear team,
is there e serial resistor needed to protect the IN_1 and IN_2 of DVR8872-Q1? Is there an ESD Structure in front of the pull down that needs to be protected or can we jus rely on the internal pull down resistors itself…
Part Number: DRV8871-Q1 Other Parts Discussed in Thread: DRV8872-Q1 , , DRV8871 Hi~
Customer is looking for high temperature operating motor drive which can support up to 120deg.
I found proper device DRV8871-Q1(DRV8872-Q1) on web site, but I don't have…
Part Number: DRV8872-Q1 Dear team,
DRV8872-Q1 has internal 100k pull down resistors on the input pins IN1 and IN2. What is the minimum and the maximum value we have to assume for this typical value of 100kOhm?
thanks
Lutz