Part Number: DRV8873 Hello everyone,
I am currently designing a compact, high-performance mobile robot using the DRV8873 (DRV8873HPWPR) in hardware mode to drive a single brushed DC motor powered from a 7–12 V battery (VM) . The motor driver is controlled…
Part Number: DRV8873 Tool/software:
I wanted to know when i command from IN1=High and IN2=Low to IN1=In2=High....recirculation initially through Body diode of FET and after dead time it does through the OUT2 HS FET right??
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 In our setup, we have provided an external switch in series with the motor/load. We open this switch intentionally to create an open-load condition and verify the OLA detection. We are observing…
Part Number: DRV8873 Hi Experts,
I need help with the issue below:
The DRV8873 is used to control a bi-directional electromagnetic lock that operates at 12V, 6A. DRV8873 was set to hardware PWM mode. The nOL and nITRIP pins are connected to DVDD through…
Part Number: DRV8873-Q1 Hi Teams,
The frequency spreading function of DRV8873-Q1 is mentioned in the datasheet.
Which register should be changed for this? It seems that there is no detailed information in the datasheet. Is there any other relevant…
Part Number: DRV8873-Q1
Tool/software:
I'm planning to design a galvanometer's galvo motor using the DRV8873-Q1.
Would you provide any related information or an EVM?
Part Number: DRV8873 Tool/software: Hi, I am using the DRV8873 driver controlled by an STM32 microcontroller. I am using it in PH EN mode at a frequency of 10kHz and with a current absorption of about 2.2 A. The load is a brushed motor. I have a problem…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 , DRV8244-Q1 , DRV8242-Q1 , DRV8243-Q1 Hello Team,
Currently we are looking for spice model for DRV8873-Q1. Could you please support.
Part Number: DRV8873 Other Parts Discussed in Thread: DRV8702-Q1 , DRV8706-Q1 , DRV8705-Q1 , DRV8703-Q1 , DRV8701 Hi Team,
I’m evaluating the DRV8873 motor driver for my project and would like your confirmation on a few points before finalizing the…
Part Number: DRV8873 Other Parts Discussed in Thread: DRV8243-Q1
Tool/software:
Hi TI team,
I’m considering using the DRV8873 to drive a DC brushed motor and would like to confirm if it is suitable for the motor I plan to use. I’ve attached the…