Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 , DRV8145-Q1 Tool/software: Hello,
I wonder if it is possible to connect multiple outputs or entire DRV8873 modules to increase the load current?
For example, combining two outputs OUT1…
Part Number: DRV8873 Tool/software: We have been using the part DRV8873SPWPRQ1 in our design for a while.
Recently in some of boards returning from the field show a unique problem.
When the H bridge is not powered and the processor does active communication…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8143-Q1 Tool/software: Hi team,
Would you please confirm whether DRV8873-Q1 could support 100kHz?
Thanks
Scarlett
Part Number: DRV8873-Q1 Tool/software: we are observing in Hardware PWM mode, fault pin is going low for every 20s. What could be the reasons? We have connected the load also.
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8242-Q1 , DRV8243-Q1 Tool/software: Hi,
I would like to use the hardware version of the device to control a motor, but without using a microcontroller. I can see one problem with this:
Since…
Part Number: DRV8873 Other Parts Discussed in Thread: DRV8212 , DRV8837 Tool/software: Hi, dear.
Sorry for troubling you.
I use DRV8873 as a simple switch for a resistive load. There is my design as below:
In the picture, the right section of ADC1 is used…
Part Number: DRV8873-Q1 Tool/software: Hello, I'm raising this question to eliminate the possibility of a dye change or a functionality modification on this part, since we've compared an old sample where the part has a visible "TI" logo and different…
Part Number: DRV8873 Tool/software: Hi Team,
Looking at the DRV8873 nSLEEP VIH,min. In the datasheet, it's listed with the other digital IO pins that says 1.6V, but also has its own section that says 2.7V. Which one is correct?
Part Number: DRV8873-Q1 Hi,
I have question on this two setup to control a peltier module.
We would like to maintain the temperature of a DUT 40 degree celsius. So for example if the DUT goes above 50 degrees we would like to cool it down to 40 degrees…