Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 , , SN74LVC8T245-EP
Tool/software:
Subject: Urgent Help Needed: Issues with DRV8873 - Q1 H-Bridge Driver in Project
Hi Team,
We are currently integrating the DRV8873-Q1 H-bridge driver from TI…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8143-Q1 Tool/software: Hi team,
Would you please confirm whether DRV8873-Q1 could support 100kHz?
Thanks
Scarlett
Part Number: DRV8873-Q1 Tool/software: we are observing in Hardware PWM mode, fault pin is going low for every 20s. What could be the reasons? We have connected the load also.
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8242-Q1 , DRV8243-Q1 Tool/software: Hi,
I would like to use the hardware version of the device to control a motor, but without using a microcontroller. I can see one problem with this:
Since…
Part Number: DRV8873-Q1 Tool/software: Hello, I'm raising this question to eliminate the possibility of a dye change or a functionality modification on this part, since we've compared an old sample where the part has a visible "TI" logo and different…
Other Parts Discussed in Thread: DRV8873-Q1 , DRV8706-Q1 , DRV8718-Q1 , DRV8214 , DRV8714-Q1 Tool/software: Hello,
Is it possible to use the signal from the IPROPI pin to perform ripple counting of the brushed dc motor being driven by the DRV8873-Q1 or is…
Part Number: DRV8873-Q1 Hi,
I have question on this two setup to control a peltier module.
We would like to maintain the temperature of a DUT 40 degree celsius. So for example if the DUT goes above 50 degrees we would like to cool it down to 40 degrees…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873H-Q1EVM , DRV8873 , DRV8262 Tool/software: I'm trying to find information on using DRV8873-Q1 to drive a solenoid.
I ordered an DRV8873H-Q1EVM and am especially interested in using this…
Part Number: DRV8873-Q1 Tool/software: Hello,
In my application, I'm using DRV8873H to drive a resistive load with high-side configuration: output is connected to resistive load to GND.
My resistive load is about 6Ohm .
Driving signal: 200Hz with…