Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 , , SN74LVC8T245-EP
Tool/software:
Subject: Urgent Help Needed: Issues with DRV8873 - Q1 H-Bridge Driver in Project
Hi Team,
We are currently integrating the DRV8873-Q1 H-bridge…
Part Number: DRV8873-Q1 Tool/software: Hi Expert,
Have a nice day!
I have some questions about DRV8873H-Q1:
Customer use DRV8873H-Q1, after powering on, the nFault Pin will be low, but the PWM outputs normally and nsleep is high.
We do the experiment…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 Tool/software: Hi,
Is it possible to detect a short circuit offline against VBat or GND when using DRV8873?
Part Number: DRV8873-Q1 Hi,
I have question on this two setup to control a peltier module.
We would like to maintain the temperature of a DUT 40 degree celsius. So for example if the DUT goes above 50 degrees we would like to cool it down to 40 degrees…
Part Number: DRV8873-Q1 In our design, there is only one DRV8873-Q1 chip used and I want to know how to test the SPI communication between MCU and DRV8873-Q1 is OK. What I mean is that when I send fixed data to DRV8873-Q1 and DRV8873-Q1 will definitely…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8143-Q1 Tool/software: Hi team,
Would you please confirm whether DRV8873-Q1 could support 100kHz?
Thanks
Scarlett
Part Number: DRV8873-Q1 Tool/software: we are observing in Hardware PWM mode, fault pin is going low for every 20s. What could be the reasons? We have connected the load also.
Part Number: DRV8873-Q1 Tool/software: Hi -
What is deglitch time on the ITRIP user-set current regulation?
I see tOCP is rated to 3uS typical / 5uS max. Also I see IPROPI typical with max SR is 10.5uS. Is ITRIP related to either of these values?…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 Hi experts.
I am currently using the DRV8873 motor driver IC to drive a DC motor. During operation, I have noticed that there is a reverse current flow of up to 2.3A from the VM pin due…