Part Number: DRV8873-Q1 Tool/software: I am using the DRV8873-Q1 (hardware version) evaluation board to prototype a TEC Driver. I have the board setup in PH/EN mode to drive a Peltier element, there is a LC filter stage between the driver outputs and…
Other Parts Discussed in Thread: DRV8873-Q1 , DRV8706-Q1 , DRV8718-Q1 , DRV8214 , DRV8714-Q1 Tool/software: Hello,
Is it possible to use the signal from the IPROPI pin to perform ripple counting of the brushed dc motor being driven by the DRV8873…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 Hi experts.
I am writing to inquire about the DRV8873 IC and its DVDD pin. According to the datasheet, it is mentioned that DVDD has an internal regulator.
I would like to confirm if…
Part Number: DRV8873-Q1 Tool/software: Hello, I see pdf recommended that VCP pin add 1uf capacitor, but in the process of debugging found that RE interference is too large, so the VCP pin adopts the form of 1uf+220nf capacitor in parallel, the chip can…
Part Number: DRV8873-Q1 Tool/software: Hello, I'm raising this question to eliminate the possibility of a dye change or a functionality modification on this part, since we've compared an old sample where the part has a visible "TI" logo and different…
Part Number: DRV8873-Q1 How many seconds after the VM supply reaches 4.35V does the VM undervoltage lockout function activate?
When observing the waveform on an oscilloscope, the timing of the VM supply reaching 4.35V and the nFAULT pin going low was…
Part Number: DRV8873-Q1 Tool/software: Hello,
In my application, I'm using DRV8873H to drive a resistive load with high-side configuration: output is connected to resistive load to GND.
My resistive load is about 6Ohm .
Driving signal: 200Hz with…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873H-Q1EVM Hi
We are planning to use DRV8873HPWPRQ1 in our automotive project. The control i/o's would be interfaced to STM320B! microcontroller.(operated at 3.3V) We want a motor driver with…
Part Number: DRV8873-Q1 Other Parts Discussed in Thread: DRV8873 Hi, expert.
I am currently working on a circuit development project and I have a question regarding the power-on sequence for the8873 motor driver. In our circuit, we have connected the…