Part Number: DRV8873HEVM Other Parts Discussed in Thread: DRV8873 , Hi,
Since I want to operate two motors, two DRV8873s are mounted on the same board. The peripheral circuits of the two ICs (CH1, CH2) are exactly the same,
but the CH1 IC's OUTPUT does…
Part Number: DRV8873HEVM Does TI provide a driver available for interacting with the FTDI FT232RL device converting the USB commands from the computer to the UART commands of the MCU on the board? I've downloaded the GUI, but the application can't seem…
Part Number: DRV8873HEVM Other Parts Discussed in Thread: DRV8873 , TMS320F280025 , C2000WARE-MOTORCONTROL-SDK Hello, this is the first time I am trying to design a motor controller to drive two Brushed DC motor, 5A Peak current each, with voltage, current…
Part Number: DRV8873HEVM Other Parts Discussed in Thread: DRV8873H-Q1EVM Hi
Please can you provide the CE/EU Declaration of Conformity for DRV8873HEVM?
The product shows it bears the CE mark however the declaration is not available on the T.I website,
…
Part Number: DRV8873HEVM Hi team,
Here's an issue from the customer may need your help:
The DRV8873HPWPR is driving a push-bar (brushed DC) using PH/EN mode to signal EN.
Without the motor, the motor is enabled, commutated, and the voltage across…
Part Number: DRV8873HEVM Other Parts Discussed in Thread: DRV8847 Hi, I need help related to DRV8873H EVM design files. Can anyone provide me DRV8873H EVM design files? I searched TI website and even if it says that it is DRV8873H EVM files but in actual…
Part Number: DRV8873HEVM Hello,
I am having troubling getting this product working. the nFault is always low from start up. I am unable to drive an output.
I believe the cause is that VCP voltage is equal VM(28V) - 0.3V. When it should be higher than…
Part Number: DRV8873HEVM Other Parts Discussed in Thread: DRV8873SEVM ,
Hello,
We know that in the DRV8873SEVM evaluation board it is possible to limit the current (overcurrent) by updating a register through the SPI interface.
We were wondering if the…
Part Number: DRV8873HEVM Other Parts Discussed in Thread: DRV8801A-Q1 , DRV8801 , DRV8844 , DRV8873 We have designed a multi-channel solenoid valve driver with the DRV8873H-Q1.
This operates from 14.4V nominal supply and uses PWM of one or the other output…
Part Number: DRV8873HEVM Other Parts Discussed in Thread: DRV8873 I'm currently trying to test out and evaluate this device. I've contacted support but apparently need to create a forum thread in order to verify if it's defective. Upon power up and verifying…