Part Number: DRV8874 The DRV8874 datasheet states: "The internal blanking time helps to prevent voltage and current transients during output switching from effecting the current regulation. These transients may be caused by a capacitor inside the motor…
Part Number: DRV8874-Q1 Hi team,
Is there any problem to contorl PWM signal (IN1/IN2) before waiting tWAKE1 or on transition from sleep mode to active mode? We use "PWM mode".
We understand that changing this device to active mode from sleep…
Part Number: DRV8874-Q1 Hi, HW guys in this forum,
I downloaded DRV8874-Q model for simulation from: https://www.ti.com/product/DRV8874-Q1?keyMatch=DRV8874-Q1&tisearch=search-everything&usecase=GPN
I have only LT-SPICE installed on my PC, so i…
Part Number: DRV8874 Other Parts Discussed in Thread: DRV8873 , Need to construct a bus converter that takes Vin = 15V and outputs 60V or 75V depending on the turns ratio of the transformer.
Would operate the DRV8874 in EN/PH mode, driving PH with 50%…
Pablo Armet said: The diagram in the datasheet does not show the extra time required for the driver to go into decay mode.
Then the diagram is wrong, isn't it?
Part Number: DRV8874-Q1 Hi Experts,
When DRV8874-Q1 is working as direct drive forward-rotating. High side OUT1 short to GND. The nFAULT was driven LOW. What can trigger nFAULT LOW?
According to the fault condition,
The current mirror is on low side…
Part Number: DRV8874-Q1 Hello,
I was verifying the Auto-Retry mode on the OCP feature and I got these scope shots:
CH1: VM, CH2: IOUT, CH3: OUT1 CH4: nFAULT
The setup is using Auto-Retry OCP mode with an E-load trying to draw about 9A from OUT1 and OUT2…
Part Number: DRV8874-Q1 I found out the wire bonding of DRV8874QPWPRQ1 is consisting of Cu.
Can you please confirm whether we had qualified AEC-006? Thank you.
Part Number: DRV8874-Q1 Hi team,
TI's motor drive IC DRV8874-Q1 output overcurrent protection, IPROPI pin configuration resistor sets the maximum overcurrent, how long does Iout fall when the output current reaches Itrip? The customer would like to k…