Part Number: DRV8874-Q1 Hi team,
Do you have a pitch conversion board for HTSSOP16?
Or is it possible to get DRV8874-Q1 sample on a pitch conversion board?
Regards, Ochi
Part Number: DRV8874-Q1 Hi team,
How much withstand voltage of capacitor between CPH and CPL is needed? I would like to decide part # of charge pump capacitor. Is it possible to use 0.022uF with 16V withstand voltage capacitor?
Regards, Ochi
Part Number: DRV8874-Q1 Other Parts Discussed in Thread: DRV8876 , I am using the PSpice transient simulation model provided on your page ( www.ti.com/.../slvmcv8) for a application with fixed off-time current regulation (IMODE pin = GND) with Orcad PSpice…
Part Number: DRV8874-Q1 Hi,
I hvae some inquiry about DRV8874-Q1 if that device satisfied on customer's requirements.
Customer requirements
1. Nominal current : 0.3A - 0.7A (at 13V), stall current : 2.3A - 3.6A
2. Load : Outside folding motor that…
Rick-san,
Could you tell me how to understand "Internally Limited" - the Absolute Max Ratings value of the DRV8874-Q1's output pin current (OUT1, OUT2)? How does it work? What's the actual threshold? etc.
Best regards, Shinichi Yok…
Part Number: DRV8874-Q1 Other Parts Discussed in Thread: DRV8874EVM Hello
I`ve bought some pre-released DRV8874-Q1 for testing, according to the evaluation board of it, it can bear continuous current of 3.3A as suggested on datasheet,
but on my designed…
Part Number: DRV8874-Q1 Other Parts Discussed in Thread: DRV8874 Hi,
In datasheet of DRV8874-Q1 page no 20, it is said that typical RDS(ON) and RDS(off) values can be found in "Typical Characteristics curves", but i could not locate the curve. Please…
Part Number: DRV8874-Q1 Other Parts Discussed in Thread: DRV8874 Hey there
I am using DRV8874 for testing, about the function of Cycle-By-Cycle Current Chopping (7.3.3.2.2), datasheet mentioned 'This allows for additional control of the current chopping…
Part Number: DRV8874-Q1 Other Parts Discussed in Thread: DRV8874 Hi
In datasheet for DRV8874-Q1 i can see in page 24 "
The data sheet generally provides a recommended minimum value, but system level testing is required to determine the appropriately…