Part Number: DRV8876 Tool/software: Hi,
I have an application using DRV8876 in PH/EN Control Mode to drive a DC brushed motor with up to 100mA motor current. PH/EN doesn't allow coast mode. Now I have seen in this e2e post ( https://e2e.ti.com/support…
Part Number: DRV8876 Other Parts Discussed in Thread: DRV8231A , Tool/software: Hi Team,
I'm using DRV8876PWPR driver IC to drive the 6v DC motor and operated by 8.4 to 6V (2S1P) battery. Using datasheet, I have implemented the below schematics as my design…
Part Number: DRV8876 Tool/software: Hello team,
My customer is wondering if they can reverse the rotation, while motor is still spinning forward. (When using PH/EN control mode)
Customer is wondering if dead time is inserted automatically.
Best Regards…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8242-Q1 Tool/software: Hi team,
we want to promote a device to against NSD7312-Q1, Could you help to recommend a suitable device?
BR
Jingguo
Part Number: DRV8876 Tool/software: Hi Experts,
Nice to talk with you. DRV8876 is under evaluation on customer side.
When DRV8876 work in Hi-Z mode, could you share the leakage current for OUT? We didn't find this data in the datasheet. Thanks.
…
Part Number: DRV8876 Hi
1. It is found that PIN10 and PIN11 of the faulty DRV8876 are short-circuited, that is, OUT2 and VM are short-circuited, and the voltage drop of PIN10 and PIN11 tubes is also measured to be 0. Other peripheral circuits are normal…
Hi MInkang,
The CPUV lasts as long there is a UV condition. There is retry circuitry involved so when the UV condition is removed, operation will resume:
Best,
Keerthi
Part Number: DRV8876-Q1 We are using DRV8876QPWPRQ1 full bridge driver to drive a brushed DC motor. The brush DC motor has 3 Ohm coild resistance and 13mH inductance. Also, the is also ring varisor across the motor terminal. I have attached the specs of…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 , DRV8801
Hi team,
thanks for your support always!
I have a question that if I would like to promote out 8876 to replace 8801, does it mean i should rewrite the software again? I have searched…