Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8242-Q1 , Dear TI experts,
My customer made their schematic using DRV8876QPWPRQ1. Could you review this schematic?
(PWR is 12V, Iout is about 360mA.)
Best regards,
Chase
Part Number: DRV8876-Q1 Dear TI experts,
My customer made their first schematic using DRV8876-Q1.
In the process they added capacitor to GND line in series like the diagram below for EMI tuning.
(I deleted rest of the components due to confidential…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876EVM , DRV8876 In our design, the IMODE pin is pulled directly to ground. According to the datasheet, when IMODE is pulled low, the nFAULT response is triggered only for overcurrent conditions…
Hi Dipak,
Dipak Bhavar said: What should be the maximum applied voltage or current to safely drive the motor?
so long as the stall current of the motor does not exceed the OCP threshold and the motor driver will not hit TSD, the current is not an…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 , DRV8876EVM Tool/software: Hello Team,
I have been testing the DRV8876 for my application, as a part of it we connected VDC(+12V) to VM and negative terminal to OUTA and the GND and PGND…
Part Number: DRV8876-Q1 Tool/software: Hi team,
I have below two questions for DRV8876QPWPRQ1:
If this BDC driver is used for driving the relay coil, could it control the current? For example, start at 3.5A and maintain at 2A.
Could this current…
Part Number: DRV8876-Q1 Tool/software: Are there any recommendations for protections on the outputs of the DRV8876-Q1 device? TVS to clamp voltage transients? Diode to clamp negative voltage swings?
I am using the driver in independent PWM output control…
Part Number: DRV8876-Q1 Tool/software: hello team:
I have a question as follows:
In DRV8876-Q1 'S specification,there is some recommended external components for the device,and the R_PMODE is in one of them.
However,when an turn to Section 7.3.2…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 Tool/software: Hello Team,
I'm designing a motor drive for DC motor of power rating 12W and the input is a 12V system. I considered DRV8876 as the driver IC and it I'm following the reference…
Part Number: DRV8876-Q1 Tool/software: Hello,
In our design, we are using DRV8876-Q1.
For the IMODE selection,
IMODE selection resistors are attached.
We are using 20.5k instead of 20k and we shall use 52.3k+10k instead of 62k resistor.
Is…