Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8242-Q1 Tool/software: Hi team,
we want to promote a device to against NSD7312-Q1, Could you help to recommend a suitable device?
BR
Jingguo
Part Number: DRV8876-Q1 Hi team,
When the charge pump is in these two fault conditions of CPUV and OCP, is the charge pump in the active state?
Thanks!
Part Number: DRV8876-Q1 We are using DRV8876QPWPRQ1 full bridge driver to drive a brushed DC motor. The brush DC motor has 3 Ohm coild resistance and 13mH inductance. Also, the is also ring varisor across the motor terminal. I have attached the specs of…
Part Number: DRV8876-Q1 Hi TI.
I am using DRV8876-Q1 Pspice Model in LT Spice Software, I am Getting an Error on DRV8876-Q1 model.
Please Suggest a solutions.
ERROR:
Questionable use of curly braces in "b§e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh…
Hi David-san, Thank you for your advice. We asked the customer to refer to SLTA055 for the capacitor capacity of OUT1 and OUT2 of DRV8876-Q1. However, the customer read the capacitor capacitance caution for Switching Regulators. Does the same caution apply…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 , DRV8801
Hi team,
thanks for your support always!
I have a question that if I would like to promote out 8876 to replace 8801, does it mean i should rewrite the software again? I have searched…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 Hi team,
could you help to answer the following questions on DS? thanks
1. IMODE configuration has 4 ways, Level 4 is the most suitable for customer application (ordinary DC motor running…
Part Number: DRV8876-Q1 Hi,all
We are very sorry to bother you. In our project, the electronic lock chip DRV8876QPWPRQ1 was damaged, which was all caused by short circuit in the power part of the chip. Could you please provide the circuit diagram inside…