Part Number: DRV8876-Q1 Belows are schematics for DRV8876-Q1
There's no software, only input 12V to VM pin
PIN(VM, VCP, CPH) = 12V
Q1) What is the normal voltage range of VCP?
12V of VCP is right?
Q2) What is the normal voltage range of CPH…
Part Number: DRV8876-Q1 Hello team,
Can I ask a question for motor selection?
The system configuration is as follows, but there is a current limit to 2A for input power.
: : VBAT (12V/ 2A: current limit) -> Boost IC (24V) -> Motor driver (DRV8876…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 Dear, TI support Team. I want to switch the rotation direction while inputting PWM from the microcontroller to the driver IC in "PWM control mode".
In that case, do I need to connect…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 , , DRV8872 I was trying to do simulation for DRV8876 in LTspice giving inputs at IN1 and IN2.Whatever the input condition is I am only getting high on OUT1 and OUT2 pins. I have tried the…
Part Number: DRV8876-Q1 Hello team,
For DRV8876-Q1, could you please provide the total current consumption for 3.3V rail (I/O), except for VM?
Thanks,
Sam Lee
Part Number: DRV8876-Q1 Could you please help provide DRV8876-Q1 below information?
1.Potential Failures mode
2.Failure Rate Distribution (in %)
Thanks a lot!
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 Could you please give me DRV8876-Q1 below information?
1.Potential Failures mode
2.Failure Rate Distribution (in %)
Thanks a lot
Part Number: DRV8874-Q1 I found out the wire bonding of DRV8874QPWPRQ1 is consisting of Cu.
Can you please confirm whether we had qualified AEC-006? Thank you.
Part Number: DRV8832-Q1 Other Parts Discussed in Thread: DRV8210 , DRV8212 , DRV8210P , DRV8212P , DRV8801A-Q1 , DRV8876-Q1 , DRV8262 Tool/software: Hello Expert,
Could you please tell me maximum input frequency?
We are planning to use 20Hz to 20kHz signal…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8801-Q1 , DRV8874-Q1 , DRV8874 , Hi team
How should we control BMD motor driver as BLDC with external hall sensor?
Is DRV8776-Q1 or DRV8874-Q1 possible to use as BLDC motor driver instead of DRV8801…