Part Number: DRV8885 About setting of M0 and M1,
Are there any restrictions when switching settings during operation?
For example, Non-Circular 1/2→1/2 step→Non-Circular 1/2
Regards,
Part Number: DRV8885 Hi team,
My customer will use DRV8885 and he provided a question.
When the motor comes to a stop, a weird sound is heard.
In this case, standby and enable are left active.
Above weird sound can be disappeared when current setting…
Part Number: DRV8885 Hi, Could you tell me the maximum and minimum value of toff time? Customers want to know the operating frequency of the timing at which the Itrip is repeated. We are trying to calculate from the following formula. Fsw=1/(Tdrive+Toff) …
Part Number: DRV8885
Hi team,
Could you please help to share how to use the PWM signal to control the chopping current in DRV8885?
Should we calculate the Voltage on the C1 and then use the equation 2?
Could you share the details calculation of Vc1?
…
Part Number: DRV8885 Hi, Customers want to measure the RDS(ON) resistance of DRV8885. Could you tell me how to measure ON resistance of high side FET and low side FET? And Please tell me the measurement system and simple block diagram. Best Regards, Yusuke …
Part Number: DRV8885 Other Parts Discussed in Thread: DRV8812 , DRV8824 When the bypass capacitor capacity is increased, step-out occurs. Please tell me the mechanism. What percentage is acceptable from 0.01uF? ask.xlsx
Part Number: DRV8885 Hi,
Could you please let me know the minimum recommendation for DVDD and AVDD capacitance that include DC bias spec?
Datasheet description : Bypass to GND with a X5R or X7R, 0.47-μF, 6.3-V ceramic capacitor.
Thanks
Muk
Part Number: DRV8885 Hi team,my customer is using DRV8885.I have some question.
For the current trip accuracy, what means" IRREF = 1.0 A, 20% to 63% current setting, 1% reference resistor,–12.5% 12.5%"
Does it mean that, for example, you…
Part Number: DRV8885 Hi
My customer have some questions regarding Leakage current from control pin to VM at VM=0V.
I found the following E2E session.
I have additional questions.
1. At VM=0V and control pins (nSLEEP, Enable, STEP, DIR ) = 3.3V, Does…