Part Number: DRV8886 Other Parts Discussed in Thread: , DRV8880 Good evening We are testing the DRV8886 stepper driver in microstep configuration, using the basic circuit proposed in the datasheet. The driver is powered by 12Volts, the stepper motor is…
Part Number: DRV8886 Hello,
Our customer use the DRV8886, are considering the ripple voltage at the VM line.
The customer are considering the ripple voltage at the VM line
and will decide the value of the bulk capacitor.
The DRV8886 has two regulators…
Part Number: DRV8886 Other Parts Discussed in Thread: MSP430F5528 Tool/software: Code Composer Studio Hello, I want to drive a bipolar stepper motor using DRV8886PWP driver and the Microcontroller is MSP430F5528. I know their is a sample code for DRV8886ATEVM…
Part Number: DRV8886 Hello,
DRV8886 IC datasheet shows operating voltage is from 8 to 37V.
We are trying to connect 4" Thermal printer and tried operating voltage of 8.5V, but IC is not able to drive the motor.
DRV8886 is working at 9V for 4" thermal…
Part Number: DRV8886EVM Other Parts Discussed in Thread: DRV8886 Hi team,
Could the DRV8886 GUI support continuously repeated configuration operation?
for example, Slow up --> Constant --> slow down --> reverse direction slow up --> constant --> slow down…
Part Number: DRV8886 Other Parts Discussed in Thread: DRV8880 , DRV8846 Hi,
We are using DRV 8886 for motor driver and it's input voltage range is 8 to 37V.
Since we are operating from battery also, our requirement of input voltage range is 6 to 30V…
Part Number: DRV8886 Hi, I am attaching my design here. It is not giving me anything in the output. Currently that 100u cap is not in place since I do not have it now, I guess that should not be the cause of my issue since that is just a noise cap. I…
Other Parts Discussed in Thread: DRV8886 , ENERGIA Anyone have an Arduino or Energia sketch for controlling the DRV8886 or similar drivers with an Arduino or MSP430?
Thanks!
-DJ
Part Number: DRV8886 Hello guys,
One of my customers is evaluating DRV8886 for their new products. In the evaluation, they had the following questions. Could you please give me your comments?
Q1. On pin function table in the device datasheet(SLVSDA4), 0.47uF…