Part Number: DRV8886EVM Hi team,
Could you tell me the country of origin of DRV8886EVM? My customer would like to export the EVM to other country, so they want to know where the DRV8886EVM is manufactured (country of origin).
I would be grateful if…
Part Number: DRV8886EVM Hello team,
I would like to confirm DRV8886EVM.
If we change the R1=15k to 12k, the EVM could have 2.5A?
I understand this device recommendation for Ifs is 2.0A, so the EVM RREF = 15kohm which the current will regulated…
Part Number: DRV8886EVM Hi, Expart.
I have a question about downloading for "DRV8886EVM Firmware and GUI".
I cannot install a GUIComposerAPP.
An error message below occurred.
Do you know why I cannnot?
Best regards, Ryuji
Part Number: DRV8886EVM Other Parts Discussed in Thread: DRV8886 Hi team,
I have a question about the DRV8886EVM.
My customer has modified the DRV8886EVM so that it can be driven by the hard IF of the DRV88886 instead of the GUI operation on the PC…
Part Number: DRV8886ATEVM Other Parts Discussed in Thread: DRV8886EVM , DRV8886 , , DRV8881EEVM Hi there
I met an issue, I downloaded the DRV8886EVM Software Files/Application/Firmware to the DRV8886EVM board, then, it cannot connected to the DRV8886_EVM…
Part Number: DRV8886EVM Other Parts Discussed in Thread: DRV8886 , DRV8880 , LM317 Hi ,
I am trying to adapt this DRV8886EVM for stepper motor application with such interface as below,
36V for VM.
5V signal on/off for enable /disable of motor…
pwm frequency get from the function: f(req)=speed*360/1.8*microsteps*60; microsteps is set by Microstepping mode,may be1, 1/2 1/4, 1/8, 1/16 and so on, speed is set 30. and useing an acceleration profile, about 5 pulse to acceleration,and 5 pulse to deceleration…
Part Number: DRV8886EVM Other Parts Discussed in Thread: DRV8886 Hi team,
Could the DRV8886 GUI support continuously repeated configuration operation?
for example, Slow up --> Constant --> slow down --> reverse direction slow up --> constant --> slow…
The idea is to send commands to the board via the serial interface. For starters I would create a GUI in Windows or Linux and send serial commands such as "/1A1000R" to move to an absolute position (Hyperterminal would also work). The code needs to be…
Tamio,
DRV8886EVM firmware code is available in https://www.ti.com/lit/zip/slvc680
The firmware is uploaded to DRV8886EVM's MSP430F2617TPM to control the DRV8886. Customers can install TI code composer studio and edit the firmware. I hope that can…