Part Number: DRV8912-Q1 Tool/software: Dears,
When the outlet of one channel is under over-current protection, will the output of other channels be turned off at the same time? Or does each channel work independently? Thanks.
Part Number: DRV8912-Q1 Tool/software: Hi,
We are tying 2x channels in parallel to our load. In our 1st use case, we have both channels turning ON and OFF at the same time by utilizing the built in 200Hz PWM. For our 2nd use, we are planning to staggering…
Part Number: DRV8912-Q1 Tool/software: Hello everyone:
Using a full-bridge load to drive the motor in continuous mode, there is no problem with open circuit detection. But when the channel is operated in PWM mode, as long as the duty cycle is smaller…
Part Number: DRV8912-Q1 If the answer is more than two, like 3. How to control 3 DRV8912-Q1 by one SPI. Besides, does this motor drive pass ISO7637 standard?
Part Number: DRV8912-Q1 Other Parts Discussed in Thread: DRV8908-Q1 , <Background>
The customer has already used DRV8908-Q1 and done the software development, but now we want to promote DRV8912-Q1 to replace existing IFX‘s TLE94112.
<Questions…
Part Number: DRV8912-Q1 Hi team,
My customer is experiencing the following issue when testing the DRV8912-Q, could you please help give some comments?
Thanks.
Background: The customer drives the multi-ported valve using the DRV8912-Q1 PWM.
Problem: During…
Part Number: DRV8912-Q1
Hi Team,
Customer used stm32f103vct6 to control 3 DRV8912 chips through daisy chain. When the sleep pin was set to 1, the fault light will light up. He tried turning off the open circuit detection but still no response. The customer…
Part Number: DRV8912-Q1 Hello team,
There are 2 VM pins.
Each have the CVM1 and CVM2 respectively, so total 4 caps.
Do you recommend to use total 4 caps? or are we able to consolidate it to 2 caps(= 1 x CVM1 and 1 x CVM2 for both VM pins)?
Regards,
…