Part Number: DRV8962 Other Parts Discussed in Thread: DRV8412 , , OPA320 Hello,
I am contacting you to request technical support regarding an evolution of a motor control electronic board.
We currently have a board named DRV12, based on the DRV8412DDW…
Part Number: DRV8962 Tool/software: Hi,
We are using the DRV8962 in several of our designs for driving solenoid valves and resistive heaters. Our schematics are as per the reference design and we are operating off a 28V supply. The loads are very light…
Part Number: DRV8962 Other Parts Discussed in Thread: DRV8837 , DRV8703-Q1 Tool/software: Dear Sir/Madam,
What is recommended if I need to drive a low frequency +/-1V (no DC) sine wave 40Hz into a 33uH inductor load. The inductor DCR is 0.15ohm. Perhaps…
Part Number: DRV8962 Tool/software: I plan to parallel OUT3 and OUT4 in my DRV8962 design. Am I correct in assuming that, if I tie IN3 and IN4 high and PWM EN3 and EN4, I won't need to add series inductance to the outputs to minimize shoot-through current…
Part Number: DRV8962 Other Parts Discussed in Thread: , DRV8262
When we set the current limit to 5 A and the load current reaches the current limit DRV8962DDVR triggers fault condition . However, if we increase the programmed current limit to 7A, the…
Part Number: DRV8962 Other Parts Discussed in Thread: DRV8462 , DRV8462EVM Hi All,
What is the usable power output of the DRV8962DDVR or DRV8962VEVM?
For example, is it possible to operate it at 65V and 10A? What is the actual power limit for operation…
Part Number: DRV8962EVM Other Parts Discussed in Thread: DRV8962 , Hello,
I recently purchased the DRV8962EVM evaluation module to use in a project. My intention is to evaluate and use only the DRV8962 motor driver IC itself, driven directly by an external…
Part Number: DRV8962 Other Parts Discussed in Thread: DRV8262 , DRV8844 Tool/software: I'm interested in paralleling DRV8962 outputs to allow for increased current to the load. Load in this case is a 50V resistive heater. Note that one side of the load…
Part Number: DRV8962 To whom it may concern:
Hello. I wanted to ask a question about a discrepancy between the spec sheet for the DRV8962DDVR part number. I have attached the reference spec url below.
www.ti.com/.../drv8962.pdf
Previously, in…
Part Number: DRV8962 Tool/software: Hello, I have similar issue. At 24V at VM, no load, all input are pulled up, there is about 30mA consomption and the device temperature rise 30°C above the ambiant. What could be the reason ? Regards, Emil