Part Number: DS100DF410 Other Parts Discussed in Thread: SIGCONARCHITECT Hello.
I downloaded SIGCONARCHITECT to control the DS100DF410 (SigCon Architect With RTE v2.0.0.8).
However, I can't use it because the DS100DF410 profile is missing.
Where…
Part Number: DS100DF410 I have an optical module with 4 pairs input and 4 pairs output high speed signals(10Gbps) to FPGA GTH interface, the signal is CML driver, Can i use a retimer DS100DF410?
Part Number: DS100DF410 Tool/software: I have a design requirement to recondition ethernet signal before passing it over to another board through a potentially noisy environment.
Basically, the idea is this: connector -> magnetics -> (something here…
Part Number: DS100DF410 Other Parts Discussed in Thread: DS125DF1610 , DS125DF111 Tool/software: Hi,
Below is copied from the another post, are these the same input signal requirement for DS100DF410 CDR locking? Thank you!
Here are some possibilities…
Part Number: DS100DF410 Other Parts Discussed in Thread: SIGCONARCHITECT Tool/software: We are working on waveform improvement for burst and continuous signal using DS100DF410. We use SigCon Architect for configuration changes.
Question 1: When the…
Part Number: DS100DF410 Hello,
I have the similar question about XFI to SFI interconnect and I found this thread.
Is it true that I can directly connect XFI to SFI from chip to chip to make them link up?
e2e.ti.com/.../ds100df410-xfi-to-sfi-ret…
Part Number: DS100DF410
Hi Team,
Would you help review customer schematics with two DS100DF410SQ in SMBus master mode? thanks a lot.
Thanks & Regards
Eddie
Part Number: DS100DF410 Other Parts Discussed in Thread: DS110DF410 , DS125DF410 , USB2ANY Hi,
Is it possible to create a 4K HDMI- Signal Eye Monitor with DS100DF410 connected via USBANY to SigCon software ?
Best Regards
Martin
Part Number: DS125DF410 Other Parts Discussed in Thread: DS100DF410 , DS110DF410 Hello,
Can I drop DS125DF410 in place of DS100DF410 with no software changes required? The datasheet does not specify which data rate the device defaults to if register…
Part Number: DS100DF410 We have attached a schematic for a re-timer between a transceiver and an SFP+ module. Please review for any errors. Is there a need for any configuration changes?