Part Number: DS100DF410 Hello everyone
we a trying to forward a gigabit link using the DS100DF410. The setup is FPGA -> DS100DF410 -> RJ45 -> RJ45 -> DS100DF410 -> FPGA. At a later point we would like to cascade more than 2 of the DS100DF410 to forward…
Part Number: DS100DF410 Other Parts Discussed in Thread: DS100RT410 , DS110DF410 Hello,
the input parameters VTX0 - VTX2 are completely unclear.
There is a similar topic on this forum but no clear answer.
OK, if the input diff voltage should be…
Part Number: DS100DF410 Hi team,
My customer is using the DS100DF410 now. We currently connect IDT clock(get the configuration from EEPROM) and DF410 .During power up, we find the DF410 will influence the i2c bus to make the clock configuration un successful…
Part Number: DS250DF410 Other Parts Discussed in Thread: DS100DF410 Hi Team, We are designing a 10G link between two separate boards. Board 1 has Marvell's cavium processor CN8350 SOC and Board2 has TI-6638K2k SOC. The 10G link is implemented over xfi…
Part Number: DS100DF410 Other Parts Discussed in Thread: DS110DF410 , DS250DF410 Dear team,
Hope you are doing well!
Recently, my customer chose to use DS100DF410.
However, they found that the DS100DF410 interface may go up-down, which means that…
Part Number: DS100DF410 Hi,
We are using DS100DF410 part in one of our custom design and to configure the retimer module we are using the below mentioned patch in the linux kernel.
https://github.com/opennetworklinux/linux/blob/master/3.2.65-1%2Bdeb7u2…
Part Number: DS100DF410 Hi,
We are planning to use the specific part DS100DF410 in one of our design.
1. It is used for upto 10G speed
2. It is used at an ambient temperature of 105C and the maximum mentioned is 85C in datasheet.
3. Using only…
Part Number: DS100DF410 As per thread https://e2e.ti.com/support/interface-group/interface/f/interface-forum/453639/df410-support-for-2-5g-ethernet
We are using LX2160_revB platform with LSDK21.08, kernel version L5.10.35_RT .
Using DS100DF410 i2c…
Part Number: DS100DF410 Hi Team,
Customer wants to verify with us for programing guide Page 13 table22 ,by default is mute driver output ?
So meaning customer must manually enable output ?
Or instead they only need to enable output mux override…
Part Number: DS100DF410 Dear Team,
Customer are looking for CAD files of DS100DF410, but cannot find it from TI.com.
Could you share CAD with me if you have it on hand? thanks.
Ben