Part Number: DS110DF410EVM I am using SV601192-001 DSP-DONGLE_EVM to connect to the the DS110DF410EMV eval board, but the connection fails, due to "invalid address". The address in SigCon Architect matches the the EVM SMbus adress and the board is in…
Part Number: DS110DF410EVM Other Parts Discussed in Thread: USB2ANY , DS110DF410 hi
i have dowbloaded software, and update for this board,
powered up of 3.3 volts, currently drawing 80 ma
2V5 is up
2v5 led is red
SMBUS LED is green
how-ever when i plug…
Part Number: DS110DF410EVM Other Parts Discussed in Thread: DS110DF410 Hi all,
For my setup at the moment I have a 644.53125MHz input into the DS110DF410EVM PRBS on one channel through SMA and output as 10.3125MHz. This channel is setup as below.
I use…
Part Number: DS110DF410EVM Hello everyone,
I am using the re-timer board DS110DF410EVM to generate high-frequency PRBS signals (10Gbps) on all four output channels.
Unfortunately, when I try to set up register 0xFF for writing on the channels register…
Part Number: DS110DF410EVM Hi all,
I am programming the retimer device onbard the EVM through I2C with a MCU broken out from another device.
I can achieve comms with the IC successfully and performs reads and writes on the device.
For the inputs I am…
Part Number: DS110DF410EVM Other Parts Discussed in Thread: DS125DF410EVM , DS125DF1610EVM Could you provide me with the schematic of DS110DF410EVM ? I can't find it on the Internet
Hi CSC,
We unfortunately do not have any board with both the DS110DF410 retimer and an FPGA on it. You can use a different vendor's FPGA board with DS110DF410EVM by connecting the I2C bus.
Best,
Lucas
Other Parts Discussed in Thread: DS110DF410 Hello,
I see on the DS110DF410 product page that there is a EVM < http://www.ti.com/tool/ds110df410evm > and a EVK < http://www.ti.com/tool/ds110df410evk > both using the same user guide showing the same…
Hi Kenji,
I tried this in lab with a very similar setup (DPS-DONGLE-EVM and DS110DF410EVM) and did not see this issue. I also tried the DS125DF410 Sigcon Architect profile and did not encounter any issues.
Do you have any jumpers connected on the DS125DF410EVM…
Part Number: DS110DF111EVM Other Parts Discussed in Thread: DS110DF111 , LMX2595 , LMX2595EVM , DS110DF410EVM Hello,
I'm using a DS110DF111 evaluation board to generate PRBS signal on a 1 GHz input signal.
The input signal is generated using a LMX2595…