Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: DS15BR400 The package is the same, and the pinout is slightly different but it seems like it would be ok as NC pins overlap with GND or VDD.
Can you please confirm?
Part Number: DS15BR400 We are using DS15BR400TSQ in our new project and we are having some issues. While input signal looks perfectly OK, the output , however, looks like modulated input. Pre-emphasis was turned off in this measurement. We triple-checked…
Part Number: DS15BR400 Hi, support team
My customer has the questions as follow:
DS15BR400TSQ/NOPB Data sheet telling that one need to refer separate sheet in product datasheet for exposed thermal pad details of RTV package. But I could not able to find…
Part Number: DS15BR400 Dear TI associate, back in January of 2020 Lee replied back to Lindsey as:
Hi Lindsey,
The unused inputs should be tied off as listed below to ensure the outputs remain in a stable state.
IN+ = 3.3K to VDD
IN- = 3.3K to GND
This…
Part Number: DS15BR400 Other Parts Discussed in Thread: DS25BR100 Hi Team, Do we have the thermal information (Theta JC and JB) for the DS15BR400 device? Also, what would be its maximum recommended junction temperature?
Thanks in advance! Kind Regards, J…
Part Number: DS15BR400 Question 1. I want to use DS15BR400 to drive a cable. Do I need another DS15BR400 on the other side of the cable to buffer the LVDS diff pairs before going to the FPGA? Is it wrong if I do use another buffer to buffer LVDS signals…
Part Number: DS15BR400 Other Parts Discussed in Thread: DS15EA101 , Hi,
I would like to buffer a 1 Gbps single ended 1.2V signal over an FMC cable to an FPGA, I'm wondering if there would be any problems with directly connecting the single ended input to…
Part Number: DS15BR400
Hi,
Noise of 4 to 5MHz occurs in VOH and VOL. I am expecting a DC level output voltage. Is there a problem with the usage of the device? The conditions are as follows. Circuit configuration: Same as figure 5. Differential Driver DC…
Part Number: DS15BR400 Other Parts Discussed in Thread: DS15BR401 , Hello
If my understanding is right through other post , e2e.ti.com/.../2423462
My understanding: the DS15BR400 's input 100ohm internal terminate resistor will have some bad influence for…