Part Number: DS15BR400 Other Parts Discussed in Thread: DS15BR401 , Hello
If my understanding is right through other post , e2e.ti.com/.../2423462
My understanding: the DS15BR400 's input 100ohm internal terminate resistor will have some bad influence for…
Part Number: DS15BR400 Hi
I'm using DS15BR400TSQ WQFN Version.
Because of my mistake, leaved open the pin number 20 and 21.
Only Pin Number 3, 4, 6, 7 are connected to the VDD(3.3V)
Is it still working or i should connect 20 and 21 pin to VDD ?? …
Part Number: DS15BR400 Hi Team
Would you let me know the difference of below IBIS files?
1,ds15br400tsq.ibs
2,ds15br400tvs.ibs
Thanks
Best regards,
Shidara
Part Number: DS15BR400 Are the LVDS inputs failsafe (do the inputs default to a fixed value when open)?
If not, what failsafe circuit is recommended for this part?
Best Regards
Part Number: SN65LVDS95 Other Parts Discussed in Thread: DS90LV049 , , SN65LVDS96 , DS92LX1622 , DS92LX1621 , DS92LV16 , DS15BR400 For the SN65LVDS 95 Transmitter and SN65LVDS 96 Receiver, what is the best practice for terminating unused inputs and unused outputs…
Part Number: DS15BR400 I have a customer who has asked about the DS15BR400TSQ on-chip termination resistors, particularly the 100 ohm output resistors. There appears to be no spec in the datasheet regarding the tolerance of these resistors. The custo…
Part Number: DS15BR400 Other Parts Discussed in Thread: DS15BR401 Hello,
I am going to use DS15BR400 as a LVDS buffer for my system. According to DS15BR400's data sheet ( www.ti.com/.../ds15br400.pdf) , the differential inputs and outputs are internally…
Other Parts Discussed in Thread: DS15BR401 , DS15BR400 Hello
Are there any plan to release automotive qualified DS15BR400, DS15BR401? Best Regards, Ryuji Asaka
Other Parts Discussed in Thread: DS15BR400 Hi,
I would use the buffer DS15BR400 to transmit the LCD LVDS signals (1 Clock LVDS + 3 lane LVDS with 30MHz pixel clock) over a cable with shielded TP. The lines are DC_coupled and well terminated with 100 Ohm…