Part Number: DS15BR401 Tool/software: Hi Kindly Suggest an Alternate Part Number either with same or different Package for P/N: DS15BR401TSQ/NOPB with Temperature Rating of -40 to +125 or -40 to +105 as we require to use the same rated device as per our…
Part Number: DS15BR401 Other Parts Discussed in Thread: SN65LVDS93B-Q1 , DS25BR440 Hi All,
I have a question about the DS15BR401.
Can I use the DS15BR401 after the LVDS output of the SN65LVDS93B-Q1?
I would like to extend the transmission distance…
Part Number: DS15BR401 Other Parts Discussed in Thread: SN65LVDS250 , DS92LV040A , DS92001 Hi support-team,
We used two of these devices in a circuit to become bi-directional. We have signals that are AC-coupled and another circuit with DC-coupling…
Part Number: DS15BR401 Hi BU friends,
My customer used DS15BR401TSQ and met the LVDS overshot. Here is the waveform of the device. The Green wave is LVDS and the yellow is PWDN. And the LVDS output connected device has internal 100ohm termination resistance…
Part Number: DS15BR400 Other Parts Discussed in Thread: DS15BR401 , Is the die for the DS15BR400 same as the DS15BR401? From what I understand the only difference is the termination on the receive side.
Part Number: DS15BR401 Hi Team,
We would like to know N/C pins of DS15BR401TSQ(WQFN PKG).
May I connect N/C pins to VDD(3.3V) or GND?
-1,17,18pins are GND
-19,22pins are VDD(3.3V)
<Background >
I would like to mount DS15BR401TSQ on a…
Hi Fandy,
The Ds15BR401 uses a voltage mode output driver. It will drive the correct output voltage with or without a Rx termination on the far end. Still there should always be a 100 Ohm termination on the Rx side to match the transmission line impedance…
Part Number: DS15BR401 Hi team,
Could you please comment on whether we can exchange the differential signal pair (as shown below) for the concern of PCB layout routing? Thanks!
Best regards,
Sam Ting
Part Number: DS90UB948-Q1 Other Parts Discussed in Thread: DS15BR401 Hello. I have a board with a repeater based on the DS90UB948 and DS90UB947 chips and DS15BR401 buffers. The board should display images on 2 displays and connect to the next board in…