Part Number: DS15EA101 Other Parts Discussed in Thread: DS15BA101 , LMH0324 , DS30EA101 Hello,
I'm looking for simulation models for DS15BA101/DS15EA101 which i could use to simulate transmission line in hyperlinx. The only models I could find are IBIS…
Hi, Nasser,
Thanks for your kindly promotion.
Can you also inform us the below issue:
1. The max. distance of the LVDS signal transfer when we use the DS15BA101 and DS15EA101?
2. The voltage of the VPP is 750mV, but our LVDS voltage is 350mV, and we need…
Part Number: DS15EA101 Other Parts Discussed in Thread: DS25BR120 Hi Team,
My customer wants to know the skew between the parts of this device.
Please tell me the skew value.
Best Regards,
Kenji
Part Number: DS15EA101 Hello,
In figure 3 of the DS15EA101 data sheet, 1uf capacitors are used to AC couple the differential input signal to the DS15EA101.
How was the 1uF value determined?
Could a much smaller value (475pF) be used.
Thank you for co…
Part Number: DS15EA101 Hello, we are using the DS15EA101 part to capture 8b/10b differential signals after 150ft of cable. We are running at 800Mbps and have had some issues receiving good quality data. We added a 100K resistor in parallel with the 1uF…
Part Number: DS15EA101 Other Parts Discussed in Thread: DS15BA101 , DS30EA101 , DS30BA101 Tool/software: WEBENCH® Design Tools Hi Team,
I would like to simulate TX/RX performance of DS15BA101 and DS15EA101 as a pair.
TX------channel----->RX
However,…
Part Number: DS15EA101 Other Parts Discussed in Thread: DS90LV001 By the way, does anyone know what exactly EN pin does?
Have 2 lvds clocks electrically paralleled (=wire or'ed), one from a DSC1123 100MHz mems oscillator, and the other from an incoming…
Part Number: DS30EA101 Other Parts Discussed in Thread: DS15EA101 , Hi team,
Since the data rate the customer want to use this time is 1.2 Gbps, I thought DS15EA101 for 1.5 Gbps was reasonable as an equalizer, Because I did not have an evaluation kit, I purchased…
Part Number: DS15EA101 I received the qualification test summary for the subject part and see that this part was tested for latchup per JESD78. I would like to know what current level this part achieved during these tests? Thanks!