Other Parts Discussed in Thread: DS15EA101 , DS15BA101 Hola,
It's blurry specify to defined the frequency and distance in data sheet and this will causes that we cannot evaluate our transmit and receive distance!
Can anyone help to provide equations…
Other Parts Discussed in Thread: DS15EA101 First question:
When the DS15EA101 is disabled, are the outputs (pin 10,11) tri-state?
Second question:
What is the power of the DS15EA101 when it is disabled?
Third question:
My application will be supporting…
Other Parts Discussed in Thread: DS15EA101 , DS15BA101 Hello,
The DS15EA101 evaluation kit has gone obsolete. Is there a substitution?
Is the DS15EA101device also going obsolete, or is it still suitable for new designs?
Regards,
Rob Curtis
Other Parts Discussed in Thread: DS15EA101 , DS15BA101 , DS25BR110 , DS25BR120 Dear Sir,
I have a prototyp board with an FPGA two DS15BA101 and two DS15EA101.
My target is to send data out of the FPGA (LVDS 2,5V) to the DS15BA101. From there AC coupled (1uF…
Hi Vasikaran,
As previously mentioned, we can only support requests for DS15EA101 IBIS models (attached earlier in the thread). We do not have resources to generate a DS15EA101 SPICE model.
Thanks,
Michael
Part Number: DS25BR110 Other Parts Discussed in Thread: DS30EA101 , , DS15BA101 , DS25BR120 , DS30BA101 , DS15EA101 Hi,
I am looking for guidance on selecting either a DS15BA101/DS15EA101, DS30BA101/DS30EA101 or DS25BR110/DS25BR120 solution to drive a 25…
Other Parts Discussed in Thread: DS15EA101 , DS25BR110 Hi,
The DS15EA101 equalizer says within the datasheet that it does not support transformer coupling. If transformer coupling is required for my application is there a method by which this device can…
Hi Nasser,
1. So in TX I need to use DS15BA101 and for RX DS15EA101, right? is it a different components and I need to order two different catalog numbers?
2. The equation doesn't take into account the VCC(operating voltage of the device) - is it ok?…