Thomas,
Please attach measurements of the clock waveform at the source and clock receive waveform at the DS16EV5110. If possible take the same measurements of the data signals too.
Thanks,
Lee
Other Parts Discussed in Thread: DS16EV5110 Hi all Would you mind if we ask DS16EV5110? If you have followings, could you send us? -S-parameter -Hspice Kind regards, Hirotaka Matsumoto
Other Parts Discussed in Thread: DS16EV5110 , DS34RT5110 , SN65DP159 Dear Sir:
Could you help kindly provide DS16EV5110 / DS34RT5110 / SN65DP159 EQ Gain v.s Frequency figure as follows?
If cannot, please help to provide EQ gain value on each data…
Part Number: DS22EV5110 Other Parts Discussed in Thread: DS16EV5110 Tool/software: Hi,
Q1. I am looking for an IC that can extend HDMI signals.
I would like an IC that can extend the signal by applying corrections to both the input and output sides…
Part Number: DS16EV5110A Other Parts Discussed in Thread: TFP401 , DS16EV5110 Tool/software: We use two DS16EV5110A to drive DVI 2560*1600@60Hz with D0~D5 data, however there is no phenomenon on the PC side with 2560*1600@60Hz edid parameter.
1) PC…
Part Number: DS16EV5110A Other Parts Discussed in Thread: DS16EV5110 Dear Sir/Madam
We’re using DS16EV5110ASQ/NOPB in our project, DS16EV5110ASQ/NOPB and was facing some error. Our HDMI output (the monitor) cannot get signal and could not display anything…
Greetings,
Per HDMI requirements, DS16EV5110 outputs must be DC coupled - 49.9-ohm to 3.3V. Output of the DS16EV5110 is open-drain and needs 3.3V pull-up resistor.
You can consider adding external 49.9-ohm pull-up to 3.3V Resistors to the DS16EV5110A…
Hi Jim,
Please note E2E case below. We only have hspice 2006 compatible ds16ev_example[1].tar.gz model only. Please attached note a copy of this model.
https://e2e.ti.com/support/interface/f/138/t/873882?tisearch=e2e-sitesearch&keymatch=ds16ev5110…