Part Number: DS25BR100 Hi there,
I am using DS25BR100 in my design. Could you help take a look of below question?
Can a 1.5V TTL signal (10MHz) inject in input pin or output in if the part is powered off? will it survive?
could you share any of…
Part Number: DS25BR100 Other Parts Discussed in Thread: DS92LV18 , DS15EA101 , DS15BA101 , Hi team,
I'm considering 300Mbps LVDS transmission using DS92LV18.
For long reach application, AN-1909 is provided as an application note. and introducing…
Part Number: DS90LV001 Hi all
My customer has a design where they have to connect two FPGAs via 2 lines at 300 Mbit. They like to use LVDS buffers and are looking at:
DS90LV001 800-Mbps LVDS buffer
DS25BR100 3.125-Gbps LVDS buffer with transmit…
Part Number: DS25BR100 Hi team,
My customer is looking for HSGMII interface redriver. I found that DS25BR100 at ti.com. Is it suitable for SGMII redriver?
Or do you have any other suggestion for it?
Part Number: DS25BR100
Hi,
Q1. I understand "Differential Input High Threshold" (VTH: +100mV (max)) as:
If the differential input voltage is 100 mV or more higher than CMR (input common mode voltage), it is not recognized as High (not guaranteed…
Part Number: DS25BR100 Hi,
We are using DS25BR100 to drive LVDS signal for 1meter cable.
While doing signal integrity with cable we are checking the LVDS waveform after 1 meter cable and it shows the amplitude is lower than expected in LVDS.
Following…
Part Number: DS25BR100 Hi TI,
I am looking for a selection guide for your repeater/redrivers (not a retimer).
The interface is CML for SGMII and possibly PCIe Gen1 or 2.
Can you help me with the selection guide and some possible selections?
Also…
Part Number: DS25BR100 Hello,
I'm looking for a LVDS buffer for 600Mbps with Ta:105C or automotive grade. For example, it could be an ideal solution if DS25BR100 covered up to 105C.
Thanks in advance.