Part Number: DS25BR440 Hi folks,
Quick question regarding the DS25BR440. On page 14 of the datasheet, the DS25BR440TSQX package has an operating temperature from -40C to 85C. However, the DS25BR440TSQ operating temperature is left blank. Can I assume…
Part Number: DS25BR440 Other Parts Discussed in Thread: DS25CP104A Hi team,
I would like to verify if it's workable to use DS25BR440 to distribute MAX9295 output LVDS signal into 4 output?
Regards,
Alex
Part Number: DS25BR440 Other Parts Discussed in Thread: DS25CP104A Hallo,
could you please send me a simulation library file for DS25BR440 or any other 3.125 Gbps LVDS Buffer with Transmit Pre-Emphasis and Receive Equalization from TI please.
Thank you …
Part Number: DS25BR440 Other Parts Discussed in Thread: DS25BR100 , , DS25BR400 , DS25BR110 Hello
we have designed an evaluation board which connects two devices using a 1.25Gbps link over 1m twisted pair cable (sgmii 8b10b).
The first device generates…
Part Number: DS25BR440 Hi,
My customer is interesting in DS25BR440TSQ/NOPB. The system turns off VDD(=3.3V) when DS25BR440 isn't used and turn on VDD when it is used. This mean is the VDD is turn on and off frequently during the system is working. It…
Part Number: DS25BR440 what might happen to the DS25BR440 if the outputs drove an open circuit with no load? For example might there be excessive to damaging ringing?
Part Number: DS25BR440 Hi,
For my design, LOS and PWDN are short together so that when LOS output LOW, the LVDS will power down. Could someone provide the following parameters: Ta, Tb, Tc and Td which are the time delay for LOS signal to response with…
Part Number: DS25BR440 Hey INT team,
I had a question regarding the DS25BR440. I'm powering the buffer wiith a 3.3V supply, but the EQ/PE/PWDN pins are powered from a different 3.3V source. Is there any problem with logic level "high" on the EQ/PE/PWDN…