Part Number: DS26LV32AT Hi Team,
In a separate thread, it is noted that the AM26LV32E is a alternative to the DS26LV32AT with a few minor difference.
My customer pointed out that the block diagrams between the two devices are not the same as the AM26LV32E…
Part Number: DS26LV32AT Hello team,
I received a question from the customer.
This is a rudimentary question, but does "Signaling rate (max) (MBits)" on the web page and "Maximum Operating Frequency" on the data sheet mean the same thing?…
Part Number: AM26LV32E Hello team,
Regarding common mode input voltage rating, +/-14V is specified as abs max rating in DS26LV32AT. There is no abs max rating for common mode input voltage specified for AM26LV32E but there is recommended range with +…
Part Number: DS26LV32AT Hi Experts,
Good day. Seeking your assistance please.
Customer needed DS26LV32ATMX/NOPB but due to unavailability, we found alternate as follows:
AM26LV32EIDR
Does this consider a drop-in replacement? Please also confirm whether…
Part Number: DS26LV32AT I have to protect against lightning and interferences telecommand and data lines RS422 which uses a DS26LV32AT as receiver. Therefore I would like a model of the receiver inputs to carry out Spice Simulations attacking the receiver…
Part Number: DS26LV32AT Hi Team,
Our customer is looking for the ESD CDM information for DS26LV32ATMX/NOPB. I checked the datasheet and HBM is the only information available.
Could you help?
Thank you.
Regards,
Marvin
Part Number: DS26LV32AT HI, Staff
For the input empty pin processing of DS26LV32ATM, there is an application document that recommends pulling up with 4.7kΩ for RI and pulling down with 4.7kΩ for R0. (2818. RS-422 Unused Inputs.pdf)
<Question…
Part Number: DS26LV32AT What is the recommended max allowable junction temperature to meet performance requirements and max allowable junction temperature to avoid damage?
Part Number: DS26LV32AT Can you please provide the theta-JA, theta-JB, theta-JC and max TJ for the DS26LV32AT?
Is there a particular place that this information is stored for easy access?
It's surprising that this info isn't in the datasheet. …
Part Number: DS26LV32AT Hi
Is it possible to provide the maximum junction temperature and thermal resistance values for the DS26LV32ATM?
Thank you!
Jim B