Part Number: DS280MB810 Hello, My customer would like to change the cross-point switch during operation by changing MUXSEL from 0 to 1 with channel A Reg_0x07[5] = channel B Reg_0x07[5] = 0 as follows. Q1: How much time does it take for the cross-point…
Part Number: DS280MB810 Hi support team, I'd like to access to DS280MB810 design documents such as S-parameter, programming guide and so on. Could you help? Best regard
Part Number: DS280MB810 Hello,
in a failure mode analysis we have identified a mode in which a Rx coax can be connected to the Tx pin.
how much of the signal on the Tx pins will be transferred to the Rx Pins in this mode?
are there any Tx to Rx suppression…
Part Number: DS280MB810 Other Parts Discussed in Thread: DS280BR810
Is there a minimum operating frequency for the DS280MB810?
This part is intended for Ethernet signals. Will it still function with regular 50% duty cycle clocks in the range of 250kHz…
Part Number: DS280MB810 Hello,
i'm searching for the SigCon Architect updater file for DS280MB810,
it is not in the SNLC056A SigCon Architect Repeater Profiles v1.1 file i've downloaded earlier today.
can anyone profide me this file?
regards…
Part Number: DS280MB810 Hello team,
Can DS280MB810 somehow operate up to 32Gbps(NRZ)?
With the device, signal will not pass at the rate? or signal will pass but it will not give enough performance as repeater?
Best regards,
Part Number: DS280MB810 Other Parts Discussed in Thread: DS280BR810 In the DS280MB810 datasheet (SNLS542, October 2016), the graphs on p. 13 in Section 6.7 show the gain transfer functions. The input differential peak-to-peak voltage is shown down to…
Part Number: DS280MB810 Other Parts Discussed in Thread: DS125BR820 , DS160PR410 Hi BU experts,
customer is looking for high speed signal(differential) repeater product like DS280MB810
Requirement :
1. Data rate: 6Gbps
2. Input/output common mode level…
Hi Wes,
While the DS280MB810 does not have a protocol dependency, it acts as a linear redriver. Depending on the signaling level, it may not be suitable as a general purpose MUX.
For example, I would expect the DS280MB810 to work for several different…