Part Number: DS64BR111 Hello,
We have approximately 20 inches of copper length on PCB (FR4) between outputs of ds64br111 to receiver (with 2 contacts on the way). The receiver has equalization on input (set to equalize 18 inch over FR4).
Can you suggest…
Part Number: DS64BR111 Other Parts Discussed in Thread: DS100BR111 , DS100BR210 Hi Team,
I am looking for a driver/buffer IC that can drive the input of SFP(4.25Gbps) transceiver. ・FPGA outputs CML signal on the board and inputs it to SFP. ・The specifications…
Part Number: DS64BR111 Hi TI,
I think I found a more suitable repeater for running 1.25Gbps SGMII in the DS64BR111.
I had some quick questions for you though:
- Do you agree that this part should work as well? Should I be able to run it using just the…
Part Number: DS64BR111 Hi,
Can DS64BR111 have different bitrates running on channel A and channel B?
Our repeater doesnt work as expected. Some disturbance is added to the output.
On the measuerments in the attached pictrue, there seems to be some peaks…
Hi Narendra,
Please consider DS64BR111. Here is the link to this part's data sheet:
https://www.ti.com/lit/ds/symlink/ds64br111.pdf?ts=1716419231046&ref_url=https%253A%252F%252Fwww.ti.com%252Fsitesearch%252Fen-us%252Fdocs%252Funiversalsearch.tsp%253FlangPref…
Part Number: DS64BR111 Hello,
I'm facing issues with the Gen2 sata connectivity.
I'm trying to make changes during the operation of the repeater and SSD connected.
First, I did a configuration of bypass mode by this set:
0x01 = FCH
0x0D = 02…
Part Number: DS64BR111 Hi Team, Our customer is requesting for the IBIS model of DS64BR111. He already tried contacting the email address in this document below but does not receive any feedback: http://www.ti.com/lit/mo/snlm143/snlm143.pdf Already tried looking…
Part Number: DS64BR111 Hello,
I was considering to use DS64BR111 until I saw that the storage temperature was -40 deg C, I need to find an alternative.
I need -55 deg C for storage.
Are there any alternative to use?
Br Mikael
Part Number: DS64BR111 Hello, I'm using the DS64BR111 and have decided to use a 3.3V supply. I just want to verify that in the 3.3V Mode the VDD pins (21,22) are ONLY connected to a 0.1uF cap to ground. Is that correct?
Last, I would like to use the…
Part Number: DS64BR111 Hi,
We will use the DS64BR111 in an fibre channel application.
Question 1:
Some of the received channels will have LVPECL. Do I need external termination for adapting to the CML input?
Question 2:
Also, on the output with CML, there…