Part Number: SN65LVDS93B Other Parts Discussed in Thread: TVP7002 , DS90C185 Hi team,
Do you have discrete solution for DE15 VGA to LVDS (Y0M、Y0P、Y1M、Y1P、Y2M、Y2P、CLKOUT_M、CLKOUT_P)?
Thanks!
Hello Elias san,
Thank you for the information.
I will infrom these device.
I could find DS90C185( serializer ) Vcc=1.8V device.
Are there any plan of deserializer which pair of DS90C185 ?
Best Regards, Ryuji Asaka
Other Parts Discussed in Thread: DS90C185 , DS90CF384 Hi,
I'am searching for a "one chip solution" to deserialize a LVDS FPD Signal in a 18 or 24bit RGB Signal.
It should be possible to connect 3D+1C or 4D+1C signalpairs.
There is a solution…
Other Parts Discussed in Thread: SN75LVDS83C , DM3730 , DS90C185 , SN65LVDS302 I have a dilema interfacing the 18-bpp to a serialiser with the DM3730. I need a 1V8 level on the DM3730 and 3v3 LVDS on the LCD side + DE,nc, nc.(ie a 21bit input to 3 chanel…
Other Parts Discussed in Thread: DS90C387 , DS90C185 Dear Sir
My client have a question about DS90C387 data mapping. They use 24 bit panel. In the datasheet data mapping as below picture.
But in the application note AN1162, data mapping as below picture…