Part Number: DS90CR287 Other Parts Discussed in Thread: DS90CR288A Hi,
There is a question aboout DS90CR287&288A.
Our camera output interface is DVP, using 8bit Data, 1 vsync signal, 1HREF signal and 1 pclock. We want to use DS90CR287 to transform DVP…
Part Number: DS90CR287 Other Parts Discussed in Thread: DS90CR482 , DS90CR481 Hello, I'm looking to do a Camera Link interface design and am looking over what parts I needs. I came across the document:
Camera_Link.pdf
Do you have any evaluation boards…
Part Number: DS90CR287 Other Parts Discussed in Thread: DS90CR288A , I want to design a full mode of cameralink. Which encoding and decoding chip is recommended?
Part Number: DS90CR287 Hi,
I'm using DS90CR287. Sometimes the start-up is abnormal. It seems that the PLL is unstable.
Do you have any suggestions about this issue?
Thanks.
Kevin Xiong
Part Number: DS90CR287 Other Parts Discussed in Thread: DS90CR288A , Hi
The customer uses DS90CR287(TX) and DS90CR288A(RX).
FPGA supplies TxCLKIN.
When FPGA is heated (at Ta=55C), TxCLKOUT has jitters and it leads data errors.
Looking into TxCLKIN, there…
Part Number: DS90CR287 I have the DS90CR287 component mounted on a board, and I would like to know if it is possible to perform an in-circuit test with a board tester mod. HP370. The test must not be performance, but ensure that the component is working…
Part Number: DS90CR287 Hello,
Our customer use the DS90CR287.
The customer change the frequency of the input clock.
So, the customer will toggle the PWR_DWN pin to reset the PLL.
How long does it take to reset the PLL?
Best Regards,
Naoki Aoyama
Part Number: DS90CR287 Other Parts Discussed in Thread: DS90CR285 , Hi
Our customer is asking why the Absolute Maximum ratings of CMOS/TTL input voltage shows different spec between DS90CR287 and DS90CR285.
DS90CR287: -0.5V to (VCC+0.3V) DS90CR285: -0.3V…