Other Parts Discussed in Thread: DS90LV012A Hi
My customer is using DS90LV012A on thier mass products in market. They have used DS90LV012A at VDD=+2.5V. But Recommended Operating Conditions is +2.7 ~ +3.6.
Could you tell me real min operating value of VDD…
To convert CMOS to CML, you can use any CML repeater (e.g., SN65CML100) and drive its input with the single-ended signal; see How to Use a 3.3-V LVDS Buffer as a Low-Voltage LVDS Driver . It's likely that you can do this directly with the SFP+ transceiver…
Other Parts Discussed in Thread: DS90LV012A I am using DS90LV012A in my design to convert a HCSL input to CMOS output. I have the below queries. The datashheet states that it can have a Vcm in the range of 0.05 to 2.35 volt . HCSL is ground referenced …
Other Parts Discussed in Thread: DS90LV011A , DS90LV012A I wonder if I can refer the equivalent schematic mode of
DS90LV011A -CMOS input -LVDS output and DS90LV012A -LVDS input. -CMOS output I want to refer them to know the ESD protection circuit structure…
Other Parts Discussed in Thread: THVD1420 , DS90LV012A , THVD1451 , THVD1552 Hello Guys,
Good day.
Do we have an LVDS to RS422 translator solution?
Thanks and regards,
Art
Part Number: DS90LV011A Other Parts Discussed in Thread: DS90LV012A Hi team,
I want to use DS90LV011A+DS90LV012A to converter the single-end signal to the differential signal, the data rate is about 1kHz. Do you think this solution can support 100m distance…
Hi Al,
Ribbon cable is generally okay for short distances (< 0.5 m). You may want to consider using the DS90LV012A and an external termination resistor instead of the DS90LT012A, as the transmission media must be terminated to its characteristic impedance…