Part Number: DS90LVRA2 Other Parts Discussed in Thread: SN74LVC2G34 Tool/software: Hi,
I need an IC that converts LVDS signal to 3.3V CMOS logic.
Thank you
Part Number: DS90LVRA2 Tool/software: Dear TI Team,
We are familiar with the DS90LV031 & 032 LVDS devices to be used on Space applications, traditional Space applications. Now, the Space business is finding new scenarios, like Constellations and New…
Part Number: DS90LVRA2-Q1 Other Parts Discussed in Thread: DS90LVRA2EVM , DS90LVRA2 Tool/software: Hi all,
I have an application that requires me to convert a 1.8V subLVDS signal to 1.8V LVCMOS (single-ended).
I'm planning on using the DS90LVRA2-Q1 part…
Part Number: DS90LVRA2 Tool/software: Hi again HSDC team,
I'm using your DS90LVRA2EVM, and I have a 120 MHz differential clock. After soldering directly to to the P/N pairs of my signal, I am only getting a much slower single-ended output at 1.8V…
Part Number: DS90LVRA2-Q1 Tool/software: 1. The Absolute Maximum Ratings of DS90LVRA2-Q1 allow for a VCC of 0V to 4V. I understand that if I set VCC to a voltage not within the range of one of the three modes lists (1.8V, 2.5V, 3.3V) that the output…
Part Number: DS90LVRA2-Q1 Tool/software: Hello,
Part D9LVRA2DEMRQ1 has below information in the datasheet regarding the input frequency
Is it maximum or this device can go further ?
If not , is there any part which supports frequency up to 400Mhz?
Regards…
Part Number: DS90LVRA2-Q1 Tool/software: Hello team,
I have a question about DS90LVRA2-Q1.
Do you have input capacitance value of the device? Vcc=1.8V.
Best regards,
Part Number: DS90LVRA2 Other Parts Discussed in Thread: SN65LVDS9638 , source is 3.3V single-ended, while target is 1.8V single-ended.
One solution to use LVDS is to shift down after LVDS receiver like in: www.ti.com/.../snla307
Would it be possible to…