Part Number: DS90UB935-Q1 Hi
My ISP outputs MIPI CSI-2 Continuous Clock mode to Serializer,
Is it necessary to configure the register 0x2[6] = 1?
It seems it works well with the register 0x2[6] = 0.
Thanks for your help.
Part Number: DS90UB953-Q1 Other Parts Discussed in Thread: DS90UB9702-Q1 , Hello TI,
I want to migrate from (DS90UB935) to DS90UB953-Q1 using same Deserializer DS90UB9702-Q1 so my question what configuration I should change to migrate.
Part Number: DS90UB935-Q1 Hi Application team:
We hear from DS90UB935-Q1 technical document introduce Spread -spectrum clocking (SSC) reduce EMI feature.
but I cannot see in the datasheet.
Is the product have the SSC function?
thank you
Part Number: DS90UB935-Q1 What is the worst-case VOL and VOH of the DS90UB935-Q1 when it is sourcing or sinking 0.4mA for a GPIO voltage of 1.8V. In datasheet VOL and VOH levels are given when sourcing/sinking a current of 4mA. In our case 935’s VOL and…
Part Number: DS90UB935-Q1 Hi Expert,
My customer is using DS90UB935 on their camera.The DS90UB935 serializer experienced a positive channel signal-less condition and a negative channel signal-good condition during an aging test at high temperature.
Analysis…
Part Number: DS90UB935-Q1 Other Parts Discussed in Thread: TPD1E01B04-Q1 Hi team,
We now have a electrostatic test problem
During the electrostatic test, if the air or contact current is ±4kV or above, video freezes will occur. The test point is any point…
Part Number: DS90UB935-Q1 Other Parts Discussed in Thread: DS90UH940-Q1 , , DS90UB940-Q1 , DS90UB936-Q1 , DS90UB949-Q1 , DS90UB941AS-Q1 Hi Experts, Good day. The customer is asking about the Compatibility of the Serializer to use for DS90UB935-Q1 and the deserializer…
Part Number: DS90UB935-Q1
In Non-Synchronous Clock Mode mode, why is the FPD-Link III forward channel rate 3 Gbps in the case of an external crystal oscillator of 52Mhz? Instead of 52x80 = 4.1Gbps? In addition, can a crystal oscillator greater than 38MHz…
Part Number: DS90UB935-Q1 We are using GPIO1 (pin no. 18) as ADC for the external voltage monitor.
We have configured the ADC code for high-level (111) and low-level (000) threshold detection.
once the voltage reaches the low-level threshold, the inter…