Part Number: DS90UB935-Q1 Other Parts Discussed in Thread: ALP Dears,
Customer want to test the DMS camera with DS90UB935&DS90UB936.The camera parameter shows below:
1.1600*1300
2.Frame rate:30
3.Data form:UYVY
Pls kindly help to provide the Configuration…
Part Number: DS90UB935-Q1
Hello FPD-LINK Expert,
May I check with you the design of POC part with you? 1. The schematic from my customer and the POC_5V waveform are attached here. As you can see POC_5V has a larger ripple when SOC resets, which is large…
Part Number: DS90UB935-Q1 Section 10.2 Layout Examples, recommends the AC-coupling capacitors be placed near the "Receiver" but this part is a Serializer (transmitter).
"The AC-coupling capacitors should be on the top layer and very close to the…
Part Number: DS90UB935-Q1 Hi team,
my customer use this mode, CLK_IN configured as 32MHz input,
use below marked GREEN to create CLK_OUT=24MHZ
then they test 32MHz active crystal : AVG: 31.997MHz, MAX: 32.051MHz, MIN: 31.948MHz.
The test CLK_OUT is…
Part Number: DS90UB935-Q1 Hi team,
my customer use this mode, CLK_IN configured as 32MHz input,
use below marked GREEN to create CLK_OUT=24MHZ
then they test 32MHz active crystal : AVG: 31.997MHz, MAX: 32.051MHz, MIN: 31.948MHz.
The test CLK_OUT is…
Part Number: DS90UB935-Q1 Hi team,
Could you please help check if there will be any risk for 24MHz external oscillator in non-sync mode?
(With 24M, customer can get their expected CLK)
In the DS, the recommend range is 25-104MHz.
Thanks,
Brian
Part Number: DS90UB935-Q1 Hi team,
As I know that we don't need to do initial setting register of 935 and 936 that SerDes will connect by themselves. However, My customer would like to know the reason about why SerDes don't need it? Would you please…