Part Number: DS90UH940N-Q1
Hello Team,
In my customer's design, BIST_EN is controlled by MCU and D_GPIO is pulled up with VDDIO for bist.
My question is that 940 can work in normal operation even D_GPIO is strapped to high when BIST EN is low by…
Part Number: DS90UH940N-Q1
Hello Team,
My customer has several question for 940N BIST option.
Could you pls help answer it??
1) For BISTC, this is for clock selection for BIST, if BISTC is enabled, internal CLK 33MHz will be used.
if so, FC rate would…
Part Number: DS90UH940N-Q1
Hello team,
LG is preparing RFQ for CCU project at GM.
One of questions is what ASIL grade 940N support.
I understand 'safety capable' means supporting ASIL-B.
I don't find any related comment on 940N datasheet. so…
Part Number: DS90UH940N-Q1 Other Parts Discussed in Thread: DS90UB941AS-Q1 DS90UH940N-Q1 FPD-LINK III RX input instability,in this unstable process use I2C to write and read register,DS90UH940N-Q1 abnormal.
(1)after abnormal, I use I2C to soft reset does…
Part Number: DS90UH940N-Q1 Hello,
According to DS90UH940N-Q1 data sheet setting RX_LOCK_MODE = 1, will result in RX-LOCK assert when device is linked to a Serializer even if active video is not being sent.
Here does it mean only the General_Status Register…
Part Number: DS90UH940N-Q1 I am using DS90UH940N-Q1。
I user applies DIGITAL_RESET0 when the serializer input signal frequency is stable to restart adaption from the minimum EQ gain value.
Write Reset Register (Address = 1h) =0x2,to AEQ。 How long it to…
Part Number: DS90UH940N-Q1 Hi team,
Could you share material content report of DS90UH940NTNKDRQ1 with PCN#20210112004.2 change ? We’ve requested it to TI CSC with request numberCS0444564 and CS0534479, however they sent us current material content report…
Part Number: DS90UH940N-Q1 Using this device as DESER and DS90UH941 as SER, I want to integrate a repeater in a Video-Chain.
DSI Clock Jitter of 941is specified as <0.3 UI-FPD, Output Clockjitter of 940 is specified as <0.35 UI. If this UI is referred…
Part Number: DS90UH940N-Q1 Other Parts Discussed in Thread: DS90UB933-Q1 Dears
May I ask which serial device is better for ds90uh940n-q1? It is 720P for the customer. Thank you!
Part Number: DS90UH940N-Q1 Other Parts Discussed in Thread: DS90UB940-Q1 Hi,
I have a question.
In DS90Ux940 or DS90Ux940N, the color space conversion from RGB to YUV is possible,
and the register value is written in "Table 9. CSI-2 Output Data Formats…