Part Number: TPS62933
We are making a cost-effective power distribution board for our drone.
The board is supposed to supply :
20A at 17.4V to a 4in1 ESC (powering 4 BLDC motors) max.
5V to flight controller at 3A max.
12V to video transmission…
Hello Deepak,
The wattage of the resistors is low as the input impedance of the sense amplifier is relatively high, so the standard 1/8th W should be sufficient.
1uF for CBST should be ok.
The 2nF capacitor in parallel to the RC compensation network seems…
Part Number: INA746 I'm coordinating design reviews through Peter James Miller
Please review my design. For this part, probably a layout review is most important. I would request to have a video chat with an engineer where I can show the layout for…
Part Number: TPS61178 TPS61178RNWR - 5V to 12V Boost, Imax ~2A
I'm coordinating design reviews through Peter James Miller
Please review my design. Schematic is shared with Peter.
Thanks!
Tom
Part Number: TUSB1210 Hi ,
As we have used one of USB Transceiver(TUSB1210) in our design we would like to hear review comments from your technical team, so that we can rectify our design.
So help in this regard.
I have attached the schematics image…
Part Number: AM6442 Hello,
We're developing a new solution with the AM6442 using the TPS6522053 PMIC. The implementation follows the SKAM64 dev board published August 22, 2022.
The design is export controlled (ITAR), so I can't post the schematic…
Part Number: TPS2121 Hello,
can I ask for a review of my design? I'm working on my bachelor thesis so any problem discovered before PCB manufacturing is welcomed.
Thank you very much!
D2 is schottky diode with 0.2 V forward voltage.
Since load capacitance…
Part Number: TPS61023 Other Parts Discussed in Thread: TPS61022 Hi,
Need design review of the below design:
VSYS can vary between 3.3V to 4.2V. Maximum output current can be 5V.
Need the output supply clean and with low noise.
Also, trying to send…
Part Number: TPS566238 Hi,
Need design review of the below design:
This circuit is used to power a LTE modem, where there is huge inrush current during startup, as high as 3A, need to make sure this circuit can handle it.
Also the input voltage can…